Skip to main content
CAPOSIENA.Philippe
Associate II
March 16, 2016
Question

Deleted file *.h with CubeMx

  • March 16, 2016
  • 3 replies
  • 768 views
Posted on March 16, 2016 at 14:47

Hello,

i'm using CubeMx 4.13 and I have this problem :

Sometimes one file *.h generated by CubeMx is deleted when regenerating the project.

In the Project settings in Code generator i use 'Generate peripherals initalization as a pair of '.c/.h' files per IP'.

I have to regenerate the project to recreate the deleted file but all my user code included is lost.

This problem happens at least once in ten and was already present in earlier version of CubeMx.

Thanks.

Philippe
    This topic has been closed for replies.

    3 replies

    Nesrine M_O
    Associate
    March 16, 2016
    Posted on March 16, 2016 at 15:19

    Hi Philippe,

    Thank you for your feedback. The issue has been reported internally.

    -Syrine-

    stm32cube-t
    ST Employee
    March 16, 2016
    Posted on March 16, 2016 at 16:04

    Dear user,

    We don't reproduce your issue. Also, can you please provide your .ioc file and indicate in which mode (standalone application, eclipse plug-in, command lines) and on which operating system you're running.

    Any specific .h file gets deleted?

     

    Thank you
    CAPOSIENA.Philippe
    Associate II
    March 18, 2016
    Posted on March 18, 2016 at 15:53

    Hello,

    here is my project. The main.c file is also rarely deleted.

    I use True Studio and my project is opened in True Studio when generating the project under CubeMx.

    The problem is very strange. Some days, no bug and some days it often happens .

    Thanks

    Philippe

    ________________

    Attachments :

    ProjectBugDeleted_hFiles.ioc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzWX&d=%2Fa%2F0X0000000bN9%2FSpqZOKcKBB3zc5ulrxTdgr8lOmQZ7wVdUghO5ceaWNc&asPdf=false