Skip to main content
gradoj
Associate
July 21, 2015
Question

STM32F4 USB minimum operating voltage

  • July 21, 2015
  • 2 replies
  • 618 views
Posted on July 21, 2015 at 22:20

I am running the stm32f407 at 1.85V and was wondering if it would be possible to get USB working at this operating voltage. I've pulled up the d+ line to Vbus but cannot get proper enumeration. I believe as long as the differential signal is 100-200mV on the receiving side it should still work. Even with a very short USB cable still no enumeration. Is some kind of level translator or usb signal repeater my only option? Thanks.

    This topic has been closed for replies.

    2 replies

    Tesla DeLorean
    Guru
    July 21, 2015
    Posted on July 21, 2015 at 22:33

    The manual for your part says 3.0V minimum VDD, and it can get down to 2.7V with degraded electrical characteristics.

    I think these are requirements of the transceiver cell itself, so I don't think you're going to be able to fudge things externally.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    gradoj
    gradojAuthor
    Associate
    July 21, 2015
    Posted on July 21, 2015 at 22:56

    Thanks. I read that minimum voltage in the datasheet as well but they explicitly said 'OTG USB FS' so I thought there may still be a chance.