Question
When will support for the STM32H7 Series be added to the MCSDK?
Posted on July 02, 2018 at 08:46
So I just ordered a IHM08M1 Nucleo BLDC motor board and what I thought would be a matching STM32H7 based Nucleo control board - only to find out from the MCSDK 5.1.1 release notes that the STM32H7 family is not supported and that the best the MCSDK supports is a NUCLEO-F446RE control board (which I have subsequently ordered - glad I didn't wait till the hardware arrived to install the SDK).
Whats the schedule for adding H7 support to the various ST libraries?
#mcsdk #stm32h7