Skip to main content
seed
Associate II
November 10, 2015
Question

DISABLE/ENABLE EXTI interrupts using hal

  • November 10, 2015
  • 4 replies
  • 9728 views
Posted on November 10, 2015 at 15:39

Hi,

I need to disable a EXTI interrupt and then enabling it again later. How can I do that using the hal implementation? I am working on STM32F070.
    This topic has been closed for replies.

    4 replies

    ftiti
    Visitor II
    November 11, 2015
    Posted on November 11, 2015 at 15:17

    You should use the Interrupt & Flag management macros existed in each peripheral .h file .

    For example to manage DMA interrupts :

    __HAL_DMA_ENABLE_IT(__HANDLE__, __INTERRUPT__);

    __HAL_DMA_EDISABLE_IT(__HANDLE__, __INTERRUPT__);

    or TIM interrupts: 

     __HAL_TIM_ENABLE_IT(__HANDLE__, __INTERRUPT__);

     __HAL_TIM_DISABLE_IT(__HANDLE__, __INTERRUPT__);

    CIAO

    seed
    seedAuthor
    Associate II
    November 11, 2015
    Posted on November 11, 2015 at 16:30

    Hi,

    The EXTI does not work the same way since it share interrupt handler with other gpio pins. I have no handle to use. See code below.

    Call stack - EXTI4_15_IRQHandler - HAL_GPIO_EXTI_IRQHandler - HAL_GPIO_EXTI_Callback.

    I want to disable interrupt on GPIO_PIN_11 for a while, how do I do that? Or should I change the gpio mode?

    I can't find something like __HAL_GPIO_EXTI_DISABLE_IT(GPIO_Pin)..

    Gpio_Init(void)

    {

     GPIO_InitTypeDef GPIO_InitStruct;

     

    ...

      __GPIOC_CLK_ENABLE();

      /*Configure GPIO pin : PC11 */

      GPIO_InitStruct.Pin = GPIO_PIN_11;

      GPIO_InitStruct.Mode = GPIO_MODE_IT_RISING;

      GPIO_InitStruct.Pull = GPIO_NOPULL;

      GPIO_InitStruct.Speed = GPIO_SPEED_LOW;

      HAL_GPIO_Init(GPIOC, &GPIO_InitStruct)

     

        /* EXTI interrupt init*/

      HAL_NVIC_SetPriority(EXTI4_15_IRQn, 0, 0);

      HAL_NVIC_EnableIRQ(EXTI4_15_IRQn);

    }  

     

    stm32f0xx_it.c

    /**

    * @brief This function handles EXTI line 4 to 15 interrupts.

    */

    void EXTI4_15_IRQHandler(void)

    {

      HAL_GPIO_EXTI_IRQHandler(GPIO_PIN_11);

    }

    stm32f0xx_hal_gpio.c

    /**

      * @brief  Handle EXTI interrupt request.

      * @param  GPIO_Pin: Specifies the port pin connected to corresponding EXTI line.

      * @retval None

      */

    void HAL_GPIO_EXTI_IRQHandler(uint16_t GPIO_Pin)

    {

      /* EXTI line interrupt detected */

      if(__HAL_GPIO_EXTI_GET_IT(GPIO_Pin) != RESET)

      {

        __HAL_GPIO_EXTI_CLEAR_IT(GPIO_Pin);

        HAL_GPIO_EXTI_Callback(GPIO_Pin);

      }

    }

    main.c

    /**

      * @brief EXTI line detection callbacks

      * @param GPIO_Pin: Specifies the pins connected EXTI line

      * @retval None

      */

    void HAL_GPIO_EXTI_Callback(uint16_t GPIO_Pin)

    {

      if (GPIO_Pin == GPIO_PIN_11)

      {

        /* OK */

      }

    }

    arik
    Visitor II
    February 2, 2016
    Posted on February 02, 2016 at 16:19

    Hi,

    Did you found a solution for that?

    How about disabling the IRQ with HAL_NVIC_DisableIRQ(EXTI4_15_IRQn) and then enabling it again when ever needed, of course it will disable all EXTI from 4 to 15 but it might help in your case.

    ABans.3
    Associate II
    November 30, 2023

    You could use something like, on test port and test pin:

     

    HAL_GPIO_DeInit(test_GPIO_Port,test_Pin);
    // disable the interuupt
    GPIO_InitTypeDef GPIO_InitStruct = {0};
    GPIO_InitStruct.Pin = test_Pin;
    GPIO_InitStruct.Pull = GPIO_PULLDOWN;
    HAL_GPIO_Init(test_GPIO_Port, &GPIO_InitStruct); // initialize it again
     
    This will disable the interrupt  on that pin. 
     
    Thanks