Skip to main content
athukuriashok
Visitor II
August 21, 2015
Question

STM32 discovery board console Port driver

  • August 21, 2015
  • 0 replies
  • 389 views
Posted on August 21, 2015 at 09:04

Hello All,

I started working/learning micripython using STM32F407 discovery board. The board I'm using is already with micropython (as my colleague used it earlier).

I connected board to Windows PC and in ST Link utility I see this:

12:24:40 : ST-LINK SN : 55FF72065075495446332087

12:24:40 : ST-LINK Firmware version : V2J23S0

12:24:40 : Connected via SWD.

12:24:40 : SWD Frequency = 1,8 MHz.

12:24:40 : Connection mode : Normal.

12:24:40 : Debug in Low Power mode enabled.

and Colored LEDs are blinking, Now I want to run few micropython commands on board. 

I connected a different USB cable at CN5 and I don't see any COM port in device manager in windows. Need help.

As of now I don't have a Linux PC to flash new binary on to the board, that's the reason I'm trying on Windows PC

Thanks

 

#micropython
    This topic has been closed for replies.