Skip to main content
Senior
September 6, 2017
Question

Is the temperature sensor integrated in STM32F429 calibrated or not?

  • September 6, 2017
  • 10 replies
  • 2155 views
Posted on September 06, 2017 at 09:59

In STM32F4's reference manual (RM0090), it gives a formula to calculate the temperature from the result converted from ADC.  But in STM32F429xxx's datasheet, I find it gives a table to show the register address store the calibration values:

0690X000006088gQAA.png

I know the temperature sensor in STM32F0 series is calibrated. So, I wonder if the temperature sensor in STM32F4 is calibrated too? 

#stm32f4 #temperature-sensor #stm32f0
This topic has been closed for replies.

10 replies

ST Technical Moderator
September 6, 2017
Posted on September 06, 2017 at 18:33

Hello

Zhang.Vincent

,

T

he temperature sensor in STM32F4 is calibrated, andyou have the calibration values in the datasheet.

Kind Regards

Imen

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Tesla DeLorean
Guru
September 6, 2017
Posted on September 06, 2017 at 18:43

>>So, I wonder if the temperature sensor in STM32F4 is calibrated too? 

But probably not in the sense that the specific device was run over temperature in an environmental chamber.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Uwe Bonnes
Chief
September 6, 2017
Posted on September 06, 2017 at 23:40

Clive,

from the datasheet I read that the chip/wafer is actually held at 30 and 110 degree and the ADC values are recorded.

john doe
Senior III
September 6, 2017
Posted on September 07, 2017 at 01:20

While it may be 'calibrated,' it is still a relative measurement and not an absolute one.

divergerAuthor
Senior
September 7, 2017
Posted on September 07, 2017 at 03:33

Can you give more explanation? I think by use the two-point calibrated data, we can get a more accurate temperature.

Tesla DeLorean
Guru
September 7, 2017
Posted on September 07, 2017 at 03:51

Precision or Accuracy?

Unless you run your chip/board/enclosure up and down across a temperature gradient to understand how your supply voltage and regulation behave, and come up with some sort of correlation, I don't think it will have much value beyond just a gate temp estimate.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..