Skip to main content
gregw
Associate
May 21, 2015
Question

VBAT circuit for STM32F429

  • May 21, 2015
  • 3 replies
  • 1726 views
Posted on May 21, 2015 at 22:20

We are using the STM32F429ZIT6 and we need to keep the RTC running when VDD is not present.  Can we hook up a coin-cell battery directly to VBAT, with no switching/monitoring circuit?  Any help would be MUCH appreciated!!

Greg
    This topic has been closed for replies.

    3 replies

    waclawek.jan
    Super User
    May 22, 2015
    Posted on May 22, 2015 at 07:54

    > We areusing the STM32F429ZIT6 and we need to keep the RTC running when VDD is not present.

    > Can we hook up a coin-cell battery directly to VBAT, with no switching/monitoring circuit?

    Yes. See the respective EVAL board (STM32439I-EVAL perhaps) for inspiration/reference (but there's nothing more than the plain battery holder connected through a jumper there).

    The gotchas are, that you are supposed to

    https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/STM32F407I%20with%20LQFP176%20%20RTC%20registers%20resets%20when%20Vbat%20below%1V&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&currentviews=42

    ; and the warning in 5.1.2 Battery backup domain chapter of RM0090 rev.9 (applies for unusually low voltage batteries only).

    Another gotcha may be the VBAT measurement in ADC, the 50k divider may suck the juice of a smaller battery quite rapidly if left connected for too long or the measurement is repeated too often.

    JW

    gregw
    gregwAuthor
    Associate
    May 22, 2015
    Posted on May 22, 2015 at 14:07

    Thanks!  This is a big help.  We'll be sure to tie VDDA to VDD and we'll also watch for any current injection into VBAT and use a diode to VDD accordingly.

    Take care...

    tm3341
    Associate III
    May 23, 2015
    Posted on May 23, 2015 at 10:42

    Actually, F4xx devices have built-in option to measure VBAT with internal ADC. You don't need to connect external resistors and everything.

    Just enable VBAT measurements by software and on some ADC channel (maybe 18) you will read VBAT value divided for some factor.

    Read datasheet for more info, Reference manual for F4xx series.