Skip to main content
Chuev.Vladimir
Associate III
February 26, 2018
Question

TrueSTUDIO: Easy to load firmware and HAL C++

  • February 26, 2018
  • 0 replies
  • 388 views
Posted on February 26, 2018 at 13:03

I'm trying to switch from Sw4stm32 to TrueSTUDIO but I have some problems.

In sw4stm32 you can easily download the firmware using the button, how can I do similar in TrueSTUDIO?

In addition, you can create a C++ project in Sw4stm32 and select the HAL, FreeRTOS, and USB HID libraries when you create it.

In TrueSTUDIO I have not found how to do this and because of this I generate the project using CubeMX, but it generates a project on C. How can I easily create a TrueSTUDIO project in C++ with the libraries I need?
    This topic has been closed for replies.