Skip to main content
zubizeratta
Associate
July 2, 2016
Question

Why Atollic Truestudio samples are removed?

  • July 2, 2016
  • 1 reply
  • 524 views
Posted on July 02, 2016 at 11:17

Hello,

I'm really wondering why Atollic Truestudio sample projects are not included with the Discovery board samples anymore?
    This topic has been closed for replies.

    1 reply

    Tesla DeLorean
    Guru
    July 2, 2016
    Posted on July 02, 2016 at 19:10

    Probably a function of uptake, and how tedious the workspace is to keep up to date, and the code regression done across a finite number of platforms. ST is also migrating to a free GNU/GCC platform.

    http://www.openstm32.org/System+Workbench+for+STM32

    If you have familiarity with the tool chain you have chosen it shouldn't take too long to standup a project from scratch. If it is hard you'd have to ask yourself why it's hard.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..