Question
STM32F4Discovery SPI1 last bit problem
Posted on September 01, 2015 at 10:35
Hello,
I have a problem with SPI1 using the STM32F4Discovery. The STM HAL(STM32Cube_FW_F4_V1.5.0 and
V1.7.0
) driver is used. When I use HAL_SPI_Transmit (master mode, bidirectional) last bit in returned byte is always zero. If I use a command with multiple returned bytes then last bit(if it is 1) go over in last bit next byte. But the same code at the SPI2 works fine. An oscilloscope shows that a slave device works properly. The problem is tested on two the
STM32F4Discovery boards.