Skip to main content
waaizkhan
Associate II
August 10, 2017
Question

quadrature encoder

Posted on August 10, 2017 at 19:48

hi everyone i have configured the timer for quadrature encoder which is working but as my quadrature encoder resolution is 1920 counts in 360 degree but in debugging mode it is give me 180 counts per 360 degree my code is given .in main function

e my code is given .in main function //for encoder initializing HAL_TIM_Encoder_Start(&htim5,TIM_CHANNEL_1|TIM_CHANNEL_2); 

while()

{

count=Encoder();

}

float Encoder(void)

{

Position=__HAL_TIM_GET_COUNTER(&htim5);

return(

Position

);

}

static void MX_TIM5_Init(void)

{

TIM_Encoder_InitTypeDef sConfig;

TIM_MasterConfigTypeDef sMasterConfig;

htim5.Instance = TIM5;

htim5.Init.Prescaler = 0;

htim5.Init.CounterMode = TIM_COUNTERMODE_UP;

htim5.Init.Period = 0xffff;

htim5.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1;

sConfig.EncoderMode = TIM_ENCODERMODE_TI2;

sConfig.IC1Polarity = TIM_ICPOLARITY_RISING;

sConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;

sConfig.IC1Prescaler = TIM_ICPSC_DIV1;

sConfig.IC1Filter = 6;

sConfig.IC2Polarity = TIM_ICPOLARITY_RISING;

sConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;

sConfig.IC2Prescaler = TIM_ICPSC_DIV1;

sConfig.IC2Filter = 6;

if (HAL_TIM_Encoder_Init(&htim5, &sConfig) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

sMasterConfig.MasterOutputTrigger = TIM_TRGO_RESET;

sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;

if (HAL_TIMEx_MasterConfigSynchronization(&htim5, &sMasterConfig) != HAL_OK)

{

_Error_Handler(__FILE__, __LINE__);

}

}

    This topic has been closed for replies.

    3 replies

    Tesla DeLorean
    Guru
    August 10, 2017
    Posted on August 10, 2017 at 20:48

    I'd recommend some cleaner initialization.

    TIM_Encoder_InitTypeDef sConfig = { 0 };

    TIM_MasterConfigTypeDef sMasterConfig = { 0 };
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Tesla DeLorean
    Guru
    August 11, 2017
    Posted on August 11, 2017 at 19:51

    STM32Cube_FW_F4_V1.16.0\Projects\STM32469I_EVAL\Examples\TIM\TIM_Encoder\Src\main.c

    /* -1- Initialize TIM1 to handle the encoder sensor */

    /* Initialize TIM1 peripheral as follows:

    + Period = 65535

    + Prescaler = 0

    + ClockDivision = 0

    + Counter direction = Up

    */

    Encoder_Handle.Instance = TIM1;

    Encoder_Handle.Init.Period = 65535;

    Encoder_Handle.Init.Prescaler = 0;

    Encoder_Handle.Init.ClockDivision = 0;

    Encoder_Handle.Init.CounterMode = TIM_COUNTERMODE_UP;

    Encoder_Handle.Init.RepetitionCounter = 0;

    sEncoderConfig.EncoderMode = TIM_ENCODERMODE_TI12;

    sEncoderConfig.IC1Polarity = TIM_ICPOLARITY_RISING;

    sEncoderConfig.IC1Selection = TIM_ICSELECTION_DIRECTTI;

    sEncoderConfig.IC1Prescaler = TIM_ICPSC_DIV1;

    sEncoderConfig.IC1Filter = 0;

    sEncoderConfig.IC2Polarity = TIM_ICPOLARITY_RISING;

    sEncoderConfig.IC2Selection = TIM_ICSELECTION_DIRECTTI;

    sEncoderConfig.IC2Prescaler = TIM_ICPSC_DIV1;

    sEncoderConfig.IC2Filter = 0;

    if(HAL_TIM_Encoder_Init(&Encoder_Handle, &sEncoderConfig) != HAL_OK)

    {

    /* Initialization Error */

    Error_Handler();

    }

    /* Start the encoder interface */

    HAL_TIM_Encoder_Start(&Encoder_Handle, TIM_CHANNEL_ALL);
    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    waaizkhan
    waaizkhanAuthor
    Associate II
    August 11, 2017
    Posted on August 11, 2017 at 18:39

    thanks a lot clive i always found u helpfull.