Skip to main content
jamann
Associate II
September 28, 2015
Question

Synchronized Output of 3 Spi with stm32f4 Discovery

  • September 28, 2015
  • 5 replies
  • 1092 views
Posted on September 28, 2015 at 19:32

Synchronized Output of 3 Spi with stm32f4 Discovery

#dma #spi #stm32f4 #discovery
This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
September 28, 2015
Posted on September 28, 2015 at 20:47

Going to be hard, can they be slaves driven by a common clock?

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jamann
jamannAuthor
Associate II
September 28, 2015
Posted on September 28, 2015 at 21:25

Somehow my initial text was not posted. I thought about SPI1 as master generating the clock and SPI2+3 as slaves. I need to feed a LED RGB Panel. SCK higher then 21Mhz doesn´t work so SDIO is not an option.

Tesla DeLorean
Guru
September 28, 2015
Posted on September 29, 2015 at 00:55

People have modulated LED signals using DMA+TIM+GPIO

The forum doesn't like mobile (tablet/phone) devices, and one wonders why Microsoft has such a time entering those markets. 

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
jamann
jamannAuthor
Associate II
September 29, 2015
Posted on September 29, 2015 at 08:13

Thank god I don´t have a microsoft phone.

Thanks for the hint. I can try DMA with GPIO

I currently use 1 SPI with DMA to drive all 3 colors daisy chained which is too slow.

I can split up the colors in 6 or maybe even 12 segments with each of them connected

to a single pin. Do you think with DMA transfer and GPIO things will go faster ?

I need at least a speedup of 4 times to achieve to get the framerate I need for 16 shades.

Tesla DeLorean
Guru
September 29, 2015
Posted on September 29, 2015 at 08:44

Have you looked at the F429I, it's got hardware for clocking video data.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..