Skip to main content
rasmusbunkenborg
Associate II
November 17, 2008
Question

ADC in dual mode setup

  • November 17, 2008
  • 2 replies
  • 680 views
Posted on November 17, 2008 at 06:52

ADC in dual mode setup

    This topic has been closed for replies.

    2 replies

    brianforde9
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:52

    Have you configured the NVIC?

    Brian F.

    rasmusbunkenborg
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:52

    Hey

    Im trying to set up the ADCs of a stm32f103rbt6 using the debugger in uvision. Its configured to run the simulation with stm32f103rb. The ADCs are supposed to run in dual mode, regular simultaneous conversion triggered by trgo3.I have enabled the eocie, and the eoc flag is set. But the program doesent jump to the interrupt vector rutine. Is there some sort trick to get it to work?

    Cheers

    Rasmus Bunkenborg

    [ This message was edited by: rasmusbunkenborg on 16-11-2008 19:25 ]