Skip to main content
rwemyss
Associate
December 25, 2008
Question

RTC clock source issues

  • December 25, 2008
  • 3 replies
  • 1041 views
Posted on December 25, 2008 at 01:07

RTC clock source issues

    This topic has been closed for replies.

    3 replies

    dschneeweis
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:54

    Hi

    I have the same problem, when using the LSI as RTC source.

    If I stop the debugger after I reseted the SEC-flag from the RTC and perform a reset with the debugger the LSEON bit is set automaticly and the LSE starts working. Now the RTC-source is choosen as LSI (because the input channel selector is in the backup-domain). The LSI itself is stopped with reset.

    The command WaitForSynchro() needs at least on tick on the RTC. But without a clocksource it waits forever.

    Why starts the LSE after clearing the SEC-flag and reset the CPU? If it wouldn't start I only had to check the LSEON bit and if not set and RTC is on start LSI.

    rwemyss
    rwemyssAuthor
    Associate
    May 17, 2011
    Posted on May 17, 2011 at 12:54

    Hey!

    I'm having some problems with the RTC on the STM32. When I use the LSE everything works as desired, but when I try to use the HSE or LSI it only works until there's a reset then stops working.

    I would expect it to work the same way for any of the clock sources. Any ideas why this is happening?

    It seems to hang on RTC_WaitForSynchro();

    I'm using a keil development board, the fwlib and basically a copy of the example given in the fwlib examples folder.

    Thanks!

    [ This message was edited by: rwemyss on 26-11-2008 18:56 ]

    pandoraems
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:54

    i am only starting with RTC stuff, but according to documentation only LSE can stay on during reset (or power off, while Vbatt is present)

    other oscillators are not a part of RTC core and therefore aren't operational in the stand-by mode.

    maybe thats the explanation to the behavior you observe?