Skip to main content
rkleine9
Associate II
November 23, 2008
Question

STM32 UART4 & UART5 On the STM3210E-EVAL Board- it doesn't work..why??

  • November 23, 2008
  • 3 replies
  • 900 views
Posted on November 23, 2008 at 16:06

STM32 UART4 & UART5 On the STM3210E-EVAL Board- it doesn't work..why??

    This topic has been closed for replies.

    3 replies

    16-32micros
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:53

    Hi Remco,

    Try first to initialize your USART/UART clocks and also the I/O ports connected to their TX and RX lines.

    Cheers,

    STOne-32.

    rkleine9
    rkleine9Author
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 12:53

    Hello,

    I'm new to the STM32 series microcontroller. I Have an STM3210E-EVAL board and tried the UARTS. UART 1 and 2 are working fine, But I cannot use the # 3,4,and 5 yet.

    I don't understand. All initialization seem to be correct, but nothing happens.... does anyone have an example using UART 4 or 5?

    I disconnected the SD card, monitored pin PC10 (UART 4 .TX), initialized alternate function pus_pull for thies pin. Enabled the clock for the UART, Enabled the UART itself... But nothing yet.

    And the first U(S)ARTS works fine both!

    Thanks in advance

    Remco

    st3
    Associate III
    May 17, 2011
    Posted on May 17, 2011 at 12:53

    Quote:

    Try first to initialize your USART/UART clocks and also the I/O ports connected to their TX and RX lines.

    I think there is a huge hole in both the STM32 documentation and the FWLib in this respect!

    The section about the USARTs in the User Manual focusses purely on the USART functionality - I can't see anywhere that details clearly, completely, and explicitly what are all the other things that also have to be set up & configured in order to actually use the USARTs! :|

    Namely:

    • The peripheral function clocks

    • The GPIO clocks

    • The GPIO alternate functions</ul>

      etc, etc...?