Question
FFT problem
Posted on January 24, 2016 at 17:45
Hi, I need do FFT on stm32f4 and therefore I
have few questions: 1. Is there any why to directly copy adc values which are uint16_t to float32_t buffer using DMA, without casting them in fork loop and using two buffers. I used this: DMA_PeripheralDataSize = DMA_PeripheralDataSize_HalfWord; DMA_MemoryDataSize = DMA_MemoryDataSize_Word; but i get only zeros. 2. I tested arm_rfft_fast_f32 function from CMSIS-DSP 1.4.4 with generated 50hz sine wave at 1000Hz sample rate using 1024 samples, but i get peek value at 102, not 51 which i should get 1000/1024 ~0,97 * 51 = 50Hz: uint16_t i; float32_t khz10[1024]; float32_t maxvalue; uint32_t maxindex; //float32_t output2[1024]; arm_rfft_fast_instance_f32 S; arm_rfft_fast_init_f32(&S, 1024); printf(''Input=[''); for(i=0; i<1024; i++){ khz10[i] = 1.2f*arm_sin_f32(2*3.1415926f*50*i/1000)+1; printf(''%f,'',khz10[i]); } printf('']\r\n''); arm_rfft_fast_f32(&S, khz10,khz10,0); arm_abs_f32(khz10, khz10, 1024); arm_max_f32(khz10+1, 1023, &maxvalue, &maxindex); printf(''Max:[%ld]:%f Output=['',maxindex,maxvalue); for(i=0; i<1024; i++){ printf(''%f,'',khz10[i]); } printf('']\r\n''); thx for help