STM32F3 opamp in PGA mode: DC conditions
Greetings
I'm trying to determine how I set the DC conditions (i.e. input bias) on the +ve input of an opamp on the STM32F3 series when all the feedback is internal during PGA mode. If I set the input to half way between the rails and set the gain at 4, the output immediately slams across to the VDD line (pretty much as expected!!).
Should I be using connected mode with the inverting input enabled and put that to the mid point of the supply and then AC couple into the +ve input pin via a capacitor?
I'm a bit lost where half my components are inside the SOC!