Skip to main content
aamzil.ilyas9
Associate
March 8, 2016
Question

STM32F407vgt problem using DCMI

Posted on March 08, 2016 at 16:02

Dear All,

I am using an stm32F4discovery ( stm324f07vgt)  to capture images coming from a camera OV5642, i would like to use DCMI but when i create a new project in STM32CubeMX to generate DCMI code, i note that there is a red ''X'' next to DCMI.

Any suggestions or advice to help me in this respect ? 

Best regards
    This topic has been closed for replies.

    2 replies

    slimen
    Visitor II
    March 8, 2016
    Posted on March 08, 2016 at 17:27

    Hello zudse.zeta,

    The DCMI pins are disabled because they are already defined and used by other external components of the board.

    To have more idea about these components, you can refer to the

    http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00039084.pdf

     User Manual, precisely in the Table 6. STM32 pin description versus board functions.

    Best Regards-ForumSTM32-

    Tesla DeLorean
    Guru
    March 8, 2016
    Posted on March 08, 2016 at 17:35

    Perhaps you want to review how the

    http://www.st.com/web/catalog/tools/FM146/CL1984/SC720/SS1462/PF255417?sc=stm32f4dis-expansion

    camera was handled, should be code of that in SPL rather than CubeMX, but might provide insight.

    CubeMX is designed to recognize pin/peripheral combinations that clash, remove the settings/configurations that clash to access the DCMI pins and peripheral.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..