cancel
Showing results for 
Search instead for 
Did you mean: 

Which STM32 series for USB HID Device?

patil
Associate II
Posted on February 16, 2016 at 15:06

Hi,

I want to develop a custom 8x8  USB hid keyboard and have studied the basics about it.

Now I am searching for USB microcontrollers supported for it.

I found STM32F0xx and STM32F1xx series both support this and also that KEIL MDK ARM toolchain for developing USB device applications is free for STM32F0xx series.

Which series microcontroller would be better  for my application?

#hid #stm32f0 #usb #stm32
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
tsuneo
Senior
Posted on February 17, 2016 at 10:02

How about NUCLEO-F042K6 board?

http://www.st.com/web/catalog/tools/FM116/SC959/SS1532/LN1847/PF262496

This board has on-board ST-Link/V2-1, 100mil-pitch pin header for each port.

The USB engine is driven by internal crystal-less clock (sync to SOF on the bus).

You'll need an extra USB connector,

For standard B receptacle,

1 VBUS - +5V (CN4-4pin)

2 D-   - PA11 (D10,CN3-13pin)

3 D+   - PA12 (D2, CN3-5pin)

4 GND  - GND (CN4-2pin)

[ CubeMX setting ]

Start New Project at File menu, and set up these items.

New Project Dialog

Click Board Selector tab - select NUCLEO-F042K6 board and push OK

Pinout tab

RCC > CRS SYNC - CRS SYNC Source USB (pull-down menu)

USB > Device (FS) (Check box)

USB_DEVICE > Class For FS IP - Human Interface Device Class (pull-down menu)

(USB_DEVICE on MiddleWare is enabled when USB - Device (FS) is checked)

Clock Configuration tab

- let CubeMX tune the setting automatically (automatic clock issues solver), following the dialog which appears when this tab is touched.

Setting finishes.

Generate Code on Project menu

Tsuneo