Skip to main content
carpenter
Visitor II
November 17, 2015
Question

Prinft and STM32F103z and STM32Cube?

  • November 17, 2015
  • 3 replies
  • 833 views
Posted on November 17, 2015 at 15:28

I start with STM32F and create my first ''Hello Word'' application a have problem with printf.

My dev.board is

http://www.waveshare.com/wiki/Open103Z

IDE Keil MDK-ARM 5.17 In the STM32Cube I create application for STM32F103Z, I set 1. RCC HSE (8MHz) 2. SYS Trace-Asynchronous_SW 3. USART1 Asynchronous 115200Bits/s 4. PF6 and PF7 set as Output (LED) Cube generate project wit this code

#include ''stm32f1xx_hal.h''
/* USER CODE BEGIN Includes */
/* USER CODE END Includes */
/* Private variables ---------------------------------------------------------*/
UART_HandleTypeDef huart1;
/* USER CODE BEGIN PV */
/* Private variables ---------------------------------------------------------*/
/* USER CODE END PV */
/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_USART1_UART_Init(void);
/* USER CODE BEGIN PFP */
/* Private function prototypes -----------------------------------------------*/
/* USER CODE END PFP */
/* USER CODE BEGIN 0 */
/* USER CODE END 0 */
int main(void)
{
/* USER CODE BEGIN 1 */
/* USER CODE END 1 */
/* MCU Configuration----------------------------------------------------------*/
/* Reset of all peripherals, Initializes the Flash interface and the Systick. */
HAL_Init();
/* Configure the system clock */
SystemClock_Config();
/* Initialize all configured peripherals */
MX_GPIO_Init();
MX_USART1_UART_Init();
/* USER CODE BEGIN 2 */
/* USER CODE END 2 */
/* Infinite loop */
/* USER CODE BEGIN WHILE */
while (1)
{
/* USER CODE END WHILE */
HAL_GPIO_TogglePin(GPIOF,GPIO_PIN_6);
printf(''Hello word!\n'');
HAL_Delay(250);
HAL_GPIO_WritePin(GPIOF,GPIO_PIN_7,GPIO_PIN_SET);
/* USER CODE BEGIN 3 */
}
/* USER CODE END 3 */
}
/** System Clock Configuration
*/
void SystemClock_Config(void)
{
RCC_OscInitTypeDef RCC_OscInitStruct;
RCC_ClkInitTypeDef RCC_ClkInitStruct;
RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSE;
RCC_OscInitStruct.HSEState = RCC_HSE_ON;
RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE;
HAL_RCC_OscConfig(&RCC_OscInitStruct);
RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_SYSCLK;
RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSE;
RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1;
RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1;
HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0);
HAL_SYSTICK_Config(HAL_RCC_GetHCLKFreq()/1000);
HAL_SYSTICK_CLKSourceConfig(SYSTICK_CLKSOURCE_HCLK);
/* SysTick_IRQn interrupt configuration */
HAL_NVIC_SetPriority(SysTick_IRQn, 0, 0);
}
/* USART1 init function */
void MX_USART1_UART_Init(void)
{
huart1.Instance = USART1;
huart1.Init.BaudRate = 115200;
huart1.Init.WordLength = UART_WORDLENGTH_8B;
huart1.Init.StopBits = UART_STOPBITS_1;
huart1.Init.Parity = UART_PARITY_NONE;
huart1.Init.Mode = UART_MODE_TX_RX;
huart1.Init.HwFlowCtl = UART_HWCONTROL_NONE;
huart1.Init.OverSampling = UART_OVERSAMPLING_16;
HAL_UART_Init(&huart1);
}
/** Configure pins as 
* Analog 
* Input 
* Output
* EVENT_OUT
* EXTI
*/
void MX_GPIO_Init(void)
{
GPIO_InitTypeDef GPIO_InitStruct;
/* GPIO Ports Clock Enable */
__GPIOC_CLK_ENABLE();
__GPIOF_CLK_ENABLE();
__GPIOA_CLK_ENABLE();
__GPIOB_CLK_ENABLE();
/*Configure GPIO pins : PF6 PF7 */
GPIO_InitStruct.Pin = GPIO_PIN_6|GPIO_PIN_7;
GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
HAL_GPIO_Init(GPIOF, &GPIO_InitStruct);
}
/* USER CODE BEGIN 4 */
/* USER CODE END 4 */
#ifdef USE_FULL_ASSERT
/**
* @brief Reports the name of the source file and the source line number
* where the assert_param error has occurred.
* @param file: pointer to the source file name
* @param line: assert_param error line source number
* @retval None
*/
void assert_failed(uint8_t* file, uint32_t line)
{
/* USER CODE BEGIN 6 */
/* User can add his own implementation to report the file name and line number,
ex: printf(''Wrong parameters value: file %s on line %d\r\n'', file, line) */
/* USER CODE END 6 */
}
#endif
/**
* @}
*/ 
/**
* @}
*/

I add my code HAL_GPIO_TogglePin(GPIOF,GPIO_PIN_6); printf(''Hello word!\n''); HAL_Delay(250); HAL_GPIO_WritePin(GPIOF,GPIO_PIN_7,GPIO_PIN_SET); LED on PF6 is lit but printf on USART1 not working

Where is the problem

?

In general,

how

to

determine

which device

(

USART1,2,3

)

will

direct the output of

printf

function?

Thank you for your help?

    This topic has been closed for replies.

    3 replies

    asrock70
    Associate III
    November 18, 2015
    Posted on November 18, 2015 at 13:40

    Must implement

    their own

    version of the function fputc()

    add this function

    int fputc(int ch, FILE *f)

    {

      HAL_UART_Transmit(&huart1, (uint8_t *)&ch, 1, 0xFFFF);

      return ch;

    }
    ckim
    Associate III
    November 26, 2015
    Posted on November 26, 2015 at 10:16

    Hi, I'm a novice to this STM32Fxx. I have a STM32F401RE board.

    I downloaded STM32Cube_FW_F4_V1.9.0 and opened a project(example using UART) coming with the package with uVision5.

    I see COM16 connected, I ran it but I don't see any print on the serial port.

    What can be wrong? (the manual says it should work.)

    Tesla DeLorean
    Guru
    November 26, 2015
    Posted on November 26, 2015 at 15:23

    What board exactly? The Nucleo?

    That would need USART2, PA2/PA3, and the aforementioned code equivalent to provide the fputc() functionality out of USART2

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..