Skip to main content
valentin
Associate III
February 10, 2016
Question

STM32F373 SDADC gain error calibration (external access to Vref_int?)

  • February 10, 2016
  • 4 replies
  • 1217 views
Posted on February 10, 2016 at 01:54

Hi!

I have been using the F373 and its SDADC successfully for a while now but in my most recent project I'd like to do a precise gain calibration without the use of additional external components.

I'm using a 3V external reference voltage connected to VREFSD+. In order to do a gain calibration, I now need to connect another known voltage < 3V to one of the analogue inputs of the same SDADC to measure the gain error.

I don't want to buy another reference IC ony for that. So my thought was if it might be possible to connect the unused internal 1.2V bandgap reference signal to one of the SDADC inputs? Basically exactly like it's done for the SAR ADC (Vrefint connected to Analog MUX):

0690X00000605LXQAY.png

In my case, it would look something like this:

0690X00000605M1QAI.png

So by measuring the internal, calibrated 1.2V bandgap voltage with the precise 3V external reference, I can calculate the exact gain and compensate any future measurements.

Unfortunately, it looks like the bandgap voltage is not accessible for the SDADC to measure, nor is it connected to any other pin.

Have I overlooked something? There must be a way to do proper gain calibration without using additional external parts?

If not, I'll use a precise resistor divider fed from 3V. But then I'm relying on their accuracy ... I'd rather like to use the calibrated internal reference.

Thanks!

Edit:

Or is there a way to use V_refint with the SAR adc so that I get the 1.2V at the VREF+ pin to route it into the SDADC?

I couldn't find any code in any examples showing that the SAR adc actually is able to use Vrefint as reference ...
    This topic has been closed for replies.

    4 replies

    valentin
    valentinAuthor
    Associate III
    February 18, 2016
    Posted on February 18, 2016 at 02:00

    *bump*

    No one any idea? Impossible? Would be so nice to have!

    valentin
    valentinAuthor
    Associate III
    February 22, 2016
    Posted on February 22, 2016 at 08:08

    Hmmkay, I take that as a ''No''. Not possible. Well then, resistor divider it is.

    Hey ST, how about you add that feature to the SDADC MUX for a next hardware revision? Just like for the SAR ADC? That would allow a nice auto-calibration when using VCC or an external voltage as Vref.

    And this makes much more sense for the SDADC, given its higher resolution ... don't you think?

    John F.
    Associate III
    February 22, 2016
    Posted on February 22, 2016 at 09:07

    The internal reference varies by + / - 3.3% over -40 .. +85 C. Would that have been good enough for you?

    From the Data Sheet:

    –40 °C < TA < +85 °C 1.16 1.20 1.24

    valentin
    valentinAuthor
    Associate III
    February 26, 2016
    Posted on February 26, 2016 at 03:53

    Hmm, does it really vary by so much when going from cold to hot?

    Or is it only the initial setpoint that can be within +/- 3.3% but stays relatively constant afterwards?

    I mean, why should STM calibrate the reference and store the data in a register if the voltage varies so much afterwards?