Skip to main content
Associate III
September 11, 2017
Question

Is there a STM8 model that has a parallel external RAM interface?

  • September 11, 2017
  • 4 replies
  • 1705 views
Posted on September 11, 2017 at 09:15

Hello. Answer please. Is there a STM8 model that has a parallel external RAM interface? Thank you in advance.

    This topic has been closed for replies.

    4 replies

    Philipp Krause
    Senior II
    October 23, 2017
    Posted on October 23, 2017 at 14:13

    Well, I guess, everyone looks at the question, doesn't know about any STM8 with parallel RAM interface (I definitely don't know about any), but are not sure that none exists, so no one answers?

    Philipp

    Associate III
    October 23, 2017
    Posted on October 23, 2017 at 16:24

    I was hoping to get a specific answer from the developers.

    Pavel A.
    October 27, 2017
    Posted on October 28, 2017 at 01:06

    Do you mean, external memory bus like in 8051? Nope :( They do not have enough pins.

    -- pa

    Associate III
    October 28, 2017
    Posted on October 28, 2017 at 06:34

    Yes. The 8-bit micro-controllers Atmel and Microchip is supported external memory interface. However, I could not find such an opportunity for STM8, even for high-density devices