Skip to main content
martinj3456
Associate III
November 28, 2017
Solved

How to differentiate USB Mass Storage and Battery charging mode: STM32L476

  • November 28, 2017
  • 2 replies
  • 1176 views
Posted on November 28, 2017 at 01:27

Hello all,

I'm using STM32L476 in a custom PCB board. Using USB OTG libary (from L4 cube examples), our code initialize USB Mass storage by following four lines of code upon USB connectivity (detected by a connected GPIO pin):

USBD_Init(&USBD_Device, &MSC_Desc, 0);                                              // USB MSC initialization

USBD_RegisterClass(&USBD_Device, USBD_MSC_CLASS);                   // USB class registration

USBD_MSC_RegisterStorage(&USBD_Device, &USBD_DISK_fops);        // Storage call backs

USBD_Start(&USBD_Device);                                                                      // Start USB MSC

We want to put the device in low power sleep mode when the USB is connected to the battery charger (not with PC for USB MSC). I request to know, how to differentiate the USB status: USB connected to PC (USB MSC initialized) vs the USB connected to wall Battery charger.

Is there any variable to look? The above functions return USBD_OK in both cases (USB connected to PC or Wall charger).

Thank you in advance for your kind reply.

    This topic has been closed for replies.
    Best answer by Ben K
    Posted on November 28, 2017 at 22:43

    1. A general approach based on the lack of host-device interaction

    2. Using the Battery Charger Detection feature

    The wall charger doesn't interact with the USB device, therefore by simply observing the 

    USBD_Device.dev_state over a couple of milliseconds you should see that instead of going to USBD_STATE_ADDRESSED and later USBD_STATE_CONFIGURED, it goes to USBD_STATE_SUSPENDED (or perhaps stays in USBD_STATE_DEFAULT).

    1. A general approach based on the lack of host-device interaction

    2. Using the Battery Charger Detection feature

    The L4 series is part of the relatively newer product lines, therefore it already has a built-in BCD feature. Unfortunately the HAL API for it is unnecessarily complicated. You should call the HAL_PCDEx_BCD_VBUSDetect() API before calling USBD_Start(). This function - instead of simply returning with the result - calls the HAL_PCDEx_BCD_Callback() callback with the determined upstream port type. Implement this callback with the following operation: call USBD_Start() when the message parameter is PCD_BCD_DISCOVERY_COMPLETED, otherwise enter the low power mode of your choosing.

    One thing to keep in mind in both cases: the physical USB connection is designed to establish power connection before the data lines. Therefore depending on the speed of plugging in the device, these detection methods require a variable delay from the time of the power connection, as they are both operational from the time the data lines are connected.

    2 replies

    Ben K
    Ben KBest answer
    Senior III
    November 28, 2017
    Posted on November 28, 2017 at 22:43

    1. A general approach based on the lack of host-device interaction

    2. Using the Battery Charger Detection feature

    The wall charger doesn't interact with the USB device, therefore by simply observing the 

    USBD_Device.dev_state over a couple of milliseconds you should see that instead of going to USBD_STATE_ADDRESSED and later USBD_STATE_CONFIGURED, it goes to USBD_STATE_SUSPENDED (or perhaps stays in USBD_STATE_DEFAULT).

    1. A general approach based on the lack of host-device interaction

    2. Using the Battery Charger Detection feature

    The L4 series is part of the relatively newer product lines, therefore it already has a built-in BCD feature. Unfortunately the HAL API for it is unnecessarily complicated. You should call the HAL_PCDEx_BCD_VBUSDetect() API before calling USBD_Start(). This function - instead of simply returning with the result - calls the HAL_PCDEx_BCD_Callback() callback with the determined upstream port type. Implement this callback with the following operation: call USBD_Start() when the message parameter is PCD_BCD_DISCOVERY_COMPLETED, otherwise enter the low power mode of your choosing.

    One thing to keep in mind in both cases: the physical USB connection is designed to establish power connection before the data lines. Therefore depending on the speed of plugging in the device, these detection methods require a variable delay from the time of the power connection, as they are both operational from the time the data lines are connected.

    martinj3456
    Associate III
    November 29, 2017
    Posted on November 29, 2017 at 05:45

    Hi Ben.

    Thank you for your direction. Yes, it worked !!! Previously I tried 1st method without the delays. 

    This time I've added a one-second delay after 

    USBD_Start(&USBD_Device);

     in the 1st method and could differentiate the USB default and configured state. Less than 1 sec did not work in my case.

    Thanks once again.

    M