Skip to main content
andre23
Associate II
August 29, 2017
Question

TIM5 TixFPx needs ~50mA to GND

  • August 29, 2017
  • 4 replies
  • 1045 views
Posted on August 29, 2017 at 21:07

Hello, I'am trying to use the TIM5 in Slave-(and Master-)Mode to drive another Timer (TIM1 to Trigger a DMA-Request on each Period).

When I configure TIM5 in Triggermode TI2FP2 on Stm32F4Discovery Board (PA1 and this is a Free IO) and Trigger Polarity falling-edge, then the Pin needs ~50mA to GND (even there, the level is few mV over zero, but enough for STM to detect the low-level).

PA1 rises to high after the 'HAL_TIM_IC_Start(&htim5,TIM_CHANNEL_2);' call.

The Datasheet tells : absolute-maximum is 25mA per Pin so this is prohibited.

The same Problem is on STM32F429 (I just tested with this two MCU's).

Can someone explain what I'am doing wrong ?

    This topic has been closed for replies.

    4 replies

    Vangelis Fortounas
    Associate II
    August 29, 2017
    Posted on August 29, 2017 at 21:24

    Hello !

    You don't provide enough details about your initialization code eg  an IOC and main.c file

    Check if  somewhere  some other code reinitialises the PA1 as an output .

    Regards..

    Vf

    Tesla DeLorean
    Guru
    August 29, 2017
    Posted on August 29, 2017 at 21:47

    Check the schematic and usability of the pin(s) in question.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    andre23
    andre23Author
    Associate II
    August 30, 2017
    Posted on August 30, 2017 at 11:10

    Initialization-Code :

    HAL_Init();

    SystemClock_Config();

    MX_GPIO_Init();

    MX_TIM5_Init();

    MX_TIM1_Init();

    HAL_TIM_IC_Start_IT(&htim1,TIM_CHANNEL_1);// this line takes no difference in problem

    HAL_TIM_IC_Start(&htim5,TIM_CHANNEL_2);

    while(1);

    Cube Configuration:

    TIM1:

    Slave Mode:Trigger Mode

    Trigger Source:TI1FP1

    Clock Source :Internal Clock

    One Pulse

    Mode: Set

    TIM5:

    Slave Mode:Trigger Mode

    Trigger Source:TI2FP2

    One Pulse Mode: Set

    In schematic is PA1 as free IO-Pin routed and PA1 and this alternate-function is for Tim5_ch2 avaliable .

    Attached: Cube-Config (Stm32F4-Discovery) + main

    ________________

    Attachments :

    stm32f407vgt6__discovery__tim5ICTrig_Test.ioc.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyRY&d=%2Fa%2F0X0000000b8H%2F_Da4kbKxpXeX8o.YLaVkwbfUsQtO9NOr4xfHhX60ykA&asPdf=false

    main.c.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HyQj&d=%2Fa%2F0X0000000b87%2FThNjbWvkyWHrMQAfRzf11pQDMoogkEeB7yd7A7RmbHA&asPdf=false
    andre23
    andre23Author
    Associate II
    August 30, 2017
    Posted on August 30, 2017 at 14:07

    OK Solved :

    HAL_TIM_OnePulse_ConfigChannel() needs to be Called , because the Input-pin is neither configured as Output or Input.

    CCMR1->CC2S was on '00' instead of '01' which is TI2FP2-Configuration