Skip to main content
T J
Senior III
June 3, 2018
Question

compiling twoo many syscalls.c ?

  • June 3, 2018
  • 1 reply
  • 486 views
Posted on June 03, 2018 at 09:10

There is syscalls.c in the Project folder generated by the cube

and in the project path, I have syscalls.c in nano libraries.

I want to sprintf with floating point, that's why I included the nano library

Trying without nano..

it compiles now...

totally clean build from the cube:

I added this into main.c and it compiles:

      printf('asd %f', 1.34);

but where does it print to ?

(Hoping to have my PCB by Tuesday for testing

:(

)

#compiler #nano
    This topic has been closed for replies.

    1 reply

    john doe
    Senior III
    June 3, 2018
    Posted on June 03, 2018 at 13:16

    I didnt think nano did floating point.  quite the opposite - i have to remove it from the options in order to print fp.

    >but where does it print to ?

    where are you telling it to print to?

    I put this in my function prototypes user code area:

    #ifdef __GNUC__

    #define PUTCHAR_PROTOTYPE int __io_putchar(int ch)

    #else

    #define PUTCHAR_PROTOTYPE int fputc(int ch, FILE *f)

    #endif /* __GNUC__ */

    and i put this in user code 4 area:

    PUTCHAR_PROTOTYPE

    {

      /* Place your implementation of fputc here */

      /* e.g. write a character to the USART2 and Loop until the end of transmission */

      HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFF);

      return ch;

    }

    the nucleo boards all seem to have the stlink on uart2, but my f769i discovery board has it on uart1.  check the manual.