Skip to main content
mbmail4
Associate III
December 18, 2017
Question

Compile time is taking forever

  • December 18, 2017
  • 1 reply
  • 591 views
Posted on December 18, 2017 at 20:18

Hi Everyone.

I recently updated my SW4STM32 IDE when prompted to do so from a pop up, and I'm now seeing its taking forever to compile a project. For example I cleaned one of my

mailto:STM#@F0

Adafruit LCD shield demo programs and then rebuilt it with the following stats finally displayed via the console view.

06:07:06 Build Finished (took 1m:46s.283ms), this is forever?

It was going through building each file one by one taking at least a second or so on each file. Is this something someone else is experiencing, can I fix this somehow?

EDIT: Also making a trivial code change produced this.

06:20:51 Build Finished (took 4s.363ms)

Thanks

mb

    This topic has been closed for replies.

    1 reply

    Alexandre Meyer
    Associate
    May 24, 2018
    Posted on May 24, 2018 at 06:10

    Hi

    B.M.002

    ‌,

    What was the code change you made to speed up compilation ?

    My full project is taking 15 minutes to compile for no special reason.

    Thanks a lot

    Alex