Skip to main content
viniciusfre
Associate II
April 10, 2018
Solved

STM32L4 - LL_USART_TransmitData8 trigger RXNE

  • April 10, 2018
  • 2 replies
  • 1458 views
Posted on April 10, 2018 at 14:27

Hello,

I am having a problem with RX interrupt. Everytime I callLL_USART_TransmitData8() it triggers RXNE flag. I enabled only RXNE , ERROR and disabled TXE. Also, If I send bytes to UART does not trigger RXNE interrupt.

I am running the firmware with freeRTOS, so maybe is a priority problem? UART priority is 6 = configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORIT(5) + 1.

void Configure_Modem_USART(void)
{
 /* Enable the peripheral clock of GPIO Port */
 MODEM_USARTx_GPIO_CLK_ENABLE();
 /* Configure Tx Pin as : Alternate function, High Speed, Push pull, Pull up */
 LL_GPIO_SetPinMode(MODEM_USARTx_TX_GPIO_PORT, MODEM_USARTx_TX_PIN, LL_GPIO_MODE_ALTERNATE);
 MODEM_USARTx_SET_TX_GPIO_AF();
 LL_GPIO_SetPinSpeed(MODEM_USARTx_TX_GPIO_PORT, MODEM_USARTx_TX_PIN, LL_GPIO_SPEED_FREQ_HIGH);
 LL_GPIO_SetPinOutputType(MODEM_USARTx_TX_GPIO_PORT, MODEM_USARTx_TX_PIN, LL_GPIO_OUTPUT_PUSHPULL);
 LL_GPIO_SetPinPull(MODEM_USARTx_TX_GPIO_PORT, MODEM_USARTx_TX_PIN, LL_GPIO_PULL_UP);
 /* Configure Rx Pin as : Alternate function, High Speed, Push pull, Pull up */
 LL_GPIO_SetPinMode(MODEM_USARTx_RX_GPIO_PORT, MODEM_USARTx_RX_PIN, LL_GPIO_MODE_ALTERNATE);
 MODEM_USARTx_SET_RX_GPIO_AF();
 LL_GPIO_SetPinSpeed(MODEM_USARTx_RX_GPIO_PORT, MODEM_USARTx_RX_PIN, LL_GPIO_SPEED_FREQ_HIGH);
 LL_GPIO_SetPinOutputType(MODEM_USARTx_RX_GPIO_PORT, MODEM_USARTx_RX_PIN, LL_GPIO_OUTPUT_PUSHPULL);
 LL_GPIO_SetPinPull(MODEM_USARTx_RX_GPIO_PORT, MODEM_USARTx_RX_PIN, LL_GPIO_PULL_UP);
 /* (2) NVIC Configuration for USART interrupts */
 /* - Set priority for USARTx_IRQn */
 /* - Enable USARTx_IRQn */
 NVIC_SetPriority(MODEM_USARTx_IRQn,
 configLIBRARY_MAX_SYSCALL_INTERRUPT_PRIORITY+1);
 NVIC_EnableIRQ(MODEM_USARTx_IRQn);
 /* (2) Enable USART peripheral clock and clock source ***********************/
 MODEM_USARTx_CLK_ENABLE();
 /* Set clock source */
 MODEM_USARTx_CLK_SOURCE();
 /* (3) Configure USART functional parameters ********************************/
 
 // HAL configuration
 USART_ModemHandle.Instance = MODEM_USARTx_INSTANCE;
USART_ModemHandle.Init.BaudRate = 115200;
USART_ModemHandle.Init.WordLength = USART_WORDLENGTH_8B;
USART_ModemHandle.Init.StopBits = USART_STOPBITS_1;
USART_ModemHandle.Init.Parity = USART_PARITY_NONE;
USART_ModemHandle.Init.Mode = UART_MODE_TX_RX;
 //USART_ModemHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
USART_ModemHandle.Init.CLKPolarity = USART_POLARITY_HIGH;
USART_ModemHandle.Init.CLKPhase = USART_PHASE_1EDGE;
USART_ModemHandle.Init.CLKLastBit = USART_LASTBIT_ENABLE;
if (HAL_USART_Init(&USART_ModemHandle) != HAL_OK) {}
/* Enable RXNE and Error interrupts, disable TX */
 LL_USART_EnableIT_RXNE(MODEM_USARTx_INSTANCE);
 LL_USART_EnableIT_ERROR(MODEM_USARTx_INSTANCE);
 LL_USART_DisableIT_TXE(MODEM_USARTx_INSTANCE);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

Interrupt handler

void MODEM_USARTx_IRQHandler(void)
{
 __IO uint32_t received_char;
 if (MODEM_USARTx_INSTANCE->ISR & USART_ISR_ORE) // Overrun Error
 MODEM_USARTx_INSTANCE->ICR = USART_ICR_ORECF;
 if (MODEM_USARTx_INSTANCE->ISR & USART_ISR_NE) // Noise Error
 MODEM_USARTx_INSTANCE->ICR = USART_ICR_NCF;
 if (MODEM_USARTx_INSTANCE->ISR & USART_ISR_FE) // Framing Error
 MODEM_USARTx_INSTANCE->ICR = USART_ICR_FECF;
 /* Check RXNE flag value in ISR register */
 if(LL_USART_IsActiveFlag_RXNE(MODEM_USARTx_INSTANCE) &&
 LL_USART_IsEnabledIT_RXNE(MODEM_USARTx_INSTANCE))
 {
 /* RXNE flag will be cleared by reading of RDR register (done in call) */
 if (idx_rx < BUF_SIZE) {
 received_char =
 LL_USART_ReceiveData8(MODEM_USARTx_INSTANCE);
 recv_buff[idx_rx++] = received_char;
 }
 else
 idx_rx = 0;
 }
 else
 {
 /* Call Error function */
 //Error_Callback();
 }
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

#freertos #stm32l4-hal #uart-rx-interrupt-routine
This topic has been closed for replies.
Best answer by viniciusfre
Posted on April 10, 2018 at 20:24

Hi,

Problem solved.For some reasonHAL_USART_Init() does not work for transmit and receive with RX interrupt enabled. I am usingLL_USART_Init() instead and works very well.

 LL_USART_InitTypeDef usart_initstruct;
 usart_initstruct.BaudRate = 115200;
 usart_initstruct.DataWidth = LL_USART_DATAWIDTH_8B;
 usart_initstruct.StopBits = LL_USART_STOPBITS_1;
 usart_initstruct.Parity = LL_USART_PARITY_NONE;
 usart_initstruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
 usart_initstruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
 usart_initstruct.OverSampling = LL_USART_OVERSAMPLING_16;
 
 /* Initialize USART instance according to parameters defined in initialization structure */
 LL_USART_Init(MODEM_USARTx_INSTANCE, &usart_initstruct);
 /* (5) Enable USART *********************************************************/
 LL_USART_Enable(MODEM_USARTx_INSTANCE);
 
 /* Polling USART initialisation */
 while((!(LL_USART_IsActiveFlag_TEACK(MODEM_USARTx_INSTANCE))) || (!(LL_USART_IsActiveFlag_REACK(MODEM_USARTx_INSTANCE))))
 { 
 }
 /* Enable RXNE and Error interrupts, disable TX */
 LL_USART_EnableIT_RXNE(MODEM_USARTx_INSTANCE);
 LL_USART_EnableIT_ERROR(MODEM_USARTx_INSTANCE);
 LL_USART_DisableIT_TXE(MODEM_USARTx_INSTANCE);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

2 replies

Tesla DeLorean
Guru
April 10, 2018
Posted on April 10, 2018 at 15:26

If you are talking to a modem you likely have ECHO turned on, use ATE0 to turn that OFF

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
viniciusfre
viniciusfreAuthorBest answer
Associate II
April 10, 2018
Posted on April 10, 2018 at 20:24

Hi,

Problem solved.For some reasonHAL_USART_Init() does not work for transmit and receive with RX interrupt enabled. I am usingLL_USART_Init() instead and works very well.

 LL_USART_InitTypeDef usart_initstruct;
 usart_initstruct.BaudRate = 115200;
 usart_initstruct.DataWidth = LL_USART_DATAWIDTH_8B;
 usart_initstruct.StopBits = LL_USART_STOPBITS_1;
 usart_initstruct.Parity = LL_USART_PARITY_NONE;
 usart_initstruct.TransferDirection = LL_USART_DIRECTION_TX_RX;
 usart_initstruct.HardwareFlowControl = LL_USART_HWCONTROL_NONE;
 usart_initstruct.OverSampling = LL_USART_OVERSAMPLING_16;
 
 /* Initialize USART instance according to parameters defined in initialization structure */
 LL_USART_Init(MODEM_USARTx_INSTANCE, &usart_initstruct);
 /* (5) Enable USART *********************************************************/
 LL_USART_Enable(MODEM_USARTx_INSTANCE);
 
 /* Polling USART initialisation */
 while((!(LL_USART_IsActiveFlag_TEACK(MODEM_USARTx_INSTANCE))) || (!(LL_USART_IsActiveFlag_REACK(MODEM_USARTx_INSTANCE))))
 { 
 }
 /* Enable RXNE and Error interrupts, disable TX */
 LL_USART_EnableIT_RXNE(MODEM_USARTx_INSTANCE);
 LL_USART_EnableIT_ERROR(MODEM_USARTx_INSTANCE);
 LL_USART_DisableIT_TXE(MODEM_USARTx_INSTANCE);�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?