Skip to main content
sjpatel19922
Associate II
March 3, 2017
Solved

Clock and PLL initialization

  • March 3, 2017
  • 3 replies
  • 2719 views
Posted on March 03, 2017 at 21:52

Hi, I amtrying to setup the clocks/PLL on the

SPC570S40E1 microcontroller.I would like use the PLL0 as the system clock.

Here is my configuration:

AC3 SC -> 16Mhz IRSOC

AC2 SC -> PLL1

PLL0 Settings:

PREDIV -> 2

MFD -> 80 RFDPHI -> 10 RFDPHI1 -> 10

PLL1 Settings:

MFD ->18 RFDPHI ->8

With the above settings, I get the following clkrates.

0690X00000606RhQAI.png

Here is my initialization code. Its getting stuck in the while loop waiting for PLL0 to lock. I am following the PLLs initializationprocedure that is recommended in the reference manual.

void spc_clock_init(void) {
 /* Waiting for IRC stabilization before attempting anything else.*/
 while (MC_ME.GS.B.S_IRC == 0U) {
 }
#if (SPC5_NO_INIT == FALSE)
#if SPC5_DISABLE_WATCHDOG
 /* SWTs disabled.*/
 SWT_2.SR.R = 0xC520U;
 SWT_2.SR.R = 0xD928U;
 SWT_2.CR.R = 0xFF000002UL;
#endif
 /* The system must be in DRUN mode on entry, if this is not the case then
 it is considered a serious anomaly.*/
 if (MC_ME.GS.B.S_CURRENT_MODE != (uint8_t)SPC5_RUNMODE_DRUN) {
 SPC5_CLOCK_FAILURE_HOOK();
 }

 /* Memory-mapped register definitions incompatible with MISRA rule. */
 /*lint -e10 -e40 -e63*/
 /* Setting the system dividers to their final values.*/
 MC_CGM.SC_DC0.R = SPC5_CGM_SC_DC0_BITS;
 MC_CGM.SC_DC1.R = SPC5_CGM_SC_DC1_BITS;
 MC_CGM.SC_DC2.R = SPC5_CGM_SC_DC2_BITS;
 
 /* Setting the auxiliary dividers to their final values.*/
 MC_CGM.AC0_DC0.R = SPC5_CGM_AC0_DC0_BITS;
 MC_CGM.AC0_DC1.R = SPC5_CGM_AC0_DC1_BITS;
 MC_CGM.AC0_DC2.R = SPC5_CGM_AC0_DC2_BITS;
 MC_CGM.AC0_DC3.R = SPC5_CGM_AC0_DC3_BITS;
 MC_CGM.AC0_DC4.R = SPC5_CGM_AC0_DC4_BITS;
 MC_CGM.AC0_DC5.R = SPC5_CGM_AC0_DC5_BITS;
 MC_CGM.AC1_DC0.R = SPC5_CGM_AC1_DC0_BITS;
 
 /* Setting the clock selectors to their final sources.*/
 MC_CGM.AC0_SC.R = SPC5_CGM_AC0_SC_BITS;
 MC_CGM.AC1_SC.R = SPC5_CGM_AC1_SC_BITS;
 MC_CGM.AC2_SC.R = SPC5_CGM_AC2_SC_BITS;
 MC_CGM.AC3_SC.R = SPC5_CGM_AC3_SC_BITS;
 /*lint +e10 +e40 +e63*/

 /* Enables the XOSC in order to check its functionality before proceeding
 with the initialization.*/
 MC_ME.DRUN_MC.R = SPC5_ME_MC_SYSCLK_IRC | SPC5_ME_MC_IRCON |
 SPC5_ME_MC_XOSCON | SPC5_ME_MC_FLAON_NORMAL |
 SPC5_ME_MC_MVRON;
 if (SPCSetRunMode(SPC5_RUNMODE_DRUN) == 0) {
 SPC5_CLOCK_FAILURE_HOOK();
 }

 // PLL0 and PLL1 initialization sequence
 // Program PLL0 Divider Register
 PLLDIG.PLL0DV.R = SPC5_PLL0_DV_RFDPHI1(SPC5_PLL0_RFDPHI1_VALUE) |
 SPC5_PLL0_DV_RFDPHI(SPC5_PLL0_RFDPHI_VALUE) |
 SPC5_PLL0_DV_PREDIV(SPC5_PLL0_PREDIV_VALUE) |
 SPC5_PLL0_DV_MFD(SPC5_PLL0_MFD_VALUE);
 // Power up PLL0
 MC_ME.DRUN_MC.B.PLL0ON = 1;
 // Poll PLL0SR[LOCK] until it asserts
 while (PLLDIG.PLL0SR.B.LOCK == 0)
 {
 }
 PLLDIG.PLL1CR.R = 0U;
 // Program PLL1 Divider Register
 PLLDIG.PLL1DV.R = SPC5_PLL1_DV_RFDPHI(SPC5_PLL1_RFDPHI_VALUE) |
 SPC5_PLL1_DV_MFD(SPC5_PLL1_MFD_VALUE);
 // Power up PLL1
 MC_ME.DRUN_MC.B.PLL1ON = 1;
 // Poll Pll1SR[LOCK] until it asserts
 while (PLLDIG.PLL1SR.B.LOCK == 0)
 {
 }
 // Engage Normal mode
 PLLDIG.PLL0CR.B.CLKCFG = 3U;
 PLLDIG.PLL1CR.B.CLKCFG = 3U;
 /* Switches to DRUN mode (current mode) in order to update the
 settings.*/
 if (SPCSetRunMode(SPC5_RUNMODE_DRUN) == 0) {
 SPC5_CLOCK_FAILURE_HOOK();
 } 
 
 /* Run modes initialization, note writes to the MC registers are verified
 by a protection mechanism, the operation success is verified at the
 end of the sequence.*/
 MC_ME.IS.R = 8U; /* Resetting I_ICONF status.*/
 MC_ME.ME.R = SPC5_ME_ME_BITS;
 MC_ME.SAFE_MC.R = SPC5_ME_SAFE_MC_BITS;
 MC_ME.DRUN_MC.R = SPC5_ME_DRUN_MC_BITS;
 MC_ME.RUN_MC[0].R = SPC5_ME_RUN0_MC_BITS;
 MC_ME.RUN_MC[1].R = SPC5_ME_RUN1_MC_BITS;
 MC_ME.RUN_MC[2].R = SPC5_ME_RUN2_MC_BITS;
 MC_ME.RUN_MC[3].R = SPC5_ME_RUN3_MC_BITS;
 MC_ME.HALT_MC.R = SPC5_ME_HALT0_MC_BITS;
 MC_ME.STOP_MC.R = SPC5_ME_STOP0_MC_BITS;
 if ((MC_ME.IS.B.I_ICONF & 1U) == 1U) {
 /* Configuration rejected.*/
 SPC5_CLOCK_FAILURE_HOOK();
 }
 /* Peripherals run and low power modes initialization.*/
 MC_ME.RUN_PC[0].R = SPC5_ME_RUN_PC0_BITS;
 MC_ME.RUN_PC[1].R = SPC5_ME_RUN_PC1_BITS;
 MC_ME.RUN_PC[2].R = SPC5_ME_RUN_PC2_BITS;
 MC_ME.RUN_PC[3].R = SPC5_ME_RUN_PC3_BITS;
 MC_ME.RUN_PC[4].R = SPC5_ME_RUN_PC4_BITS;
 MC_ME.RUN_PC[5].R = SPC5_ME_RUN_PC5_BITS;
 MC_ME.RUN_PC[6].R = SPC5_ME_RUN_PC6_BITS;
 MC_ME.RUN_PC[7].R = SPC5_ME_RUN_PC7_BITS;
 MC_ME.LP_PC[0].R = SPC5_ME_LP_PC0_BITS;
 MC_ME.LP_PC[1].R = SPC5_ME_LP_PC1_BITS;
 MC_ME.LP_PC[2].R = SPC5_ME_LP_PC2_BITS;
 MC_ME.LP_PC[3].R = SPC5_ME_LP_PC3_BITS;
 MC_ME.LP_PC[4].R = SPC5_ME_LP_PC4_BITS;
 MC_ME.LP_PC[5].R = SPC5_ME_LP_PC5_BITS;
 MC_ME.LP_PC[6].R = SPC5_ME_LP_PC6_BITS;
 MC_ME.LP_PC[7].R = SPC5_ME_LP_PC7_BITS;
 /* Switches again to DRUN mode (current mode) in order to update the
 settings.*/
 if (SPCSetRunMode(SPC5_RUNMODE_DRUN) == 0) {
 SPC5_CLOCK_FAILURE_HOOK();
 }

}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?

#spc570s
    This topic has been closed for replies.
    Best answer by zambrano.luigi
    Posted on March 09, 2017 at 13:31

    Hi, 

    about your configuration, I suppose that you have set

    AC2 SC  -> 16Mhz IRSOC

    AC3 SC  -> PLL1

    The opposite is not possible. 

    As described in the Reference Manual, any modification of the mode configuration register of the currently selected mode will not be taken into account immediately but on the next request to enter this mode (48.4.1 Mode Transition Request).

    In other words, if you want to enable the PLL0 for the DRUN mode, you have to switches again to DRUN mode in order the modification takes into account. 

    So, you have to use the following isntructions

    // Power up PLL0

    MC_ME.DRUN_MC.B.PLL0ON = 1;

    /* Switches again to DRUN mode (current mode) in order to update the

    settings.*/

    if (SPCSetRunMode(SPC5_RUNMODE_DRUN) == CLOCK_FAILED) {

    SPC5_CLOCK_FAILURE_HOOK();

    }

    // Poll PLL0SR[LOCK] until it asserts

    while (PLLDIG.PLL0SR.B.LOCK == 0)

    {

    }

    In any case, let me underline that, if you want to change the mode configuration, you can use the graphic interface (section Module Entry of the Clock Component) by enabling the Advanced Mode. 

    Regards,

    Luigi

    3 replies

    zambrano.luigi
    zambrano.luigiBest answer
    ST Employee
    March 9, 2017
    Posted on March 09, 2017 at 13:31

    Hi, 

    about your configuration, I suppose that you have set

    AC2 SC  -> 16Mhz IRSOC

    AC3 SC  -> PLL1

    The opposite is not possible. 

    As described in the Reference Manual, any modification of the mode configuration register of the currently selected mode will not be taken into account immediately but on the next request to enter this mode (48.4.1 Mode Transition Request).

    In other words, if you want to enable the PLL0 for the DRUN mode, you have to switches again to DRUN mode in order the modification takes into account. 

    So, you have to use the following isntructions

    // Power up PLL0

    MC_ME.DRUN_MC.B.PLL0ON = 1;

    /* Switches again to DRUN mode (current mode) in order to update the

    settings.*/

    if (SPCSetRunMode(SPC5_RUNMODE_DRUN) == CLOCK_FAILED) {

    SPC5_CLOCK_FAILURE_HOOK();

    }

    // Poll PLL0SR[LOCK] until it asserts

    while (PLLDIG.PLL0SR.B.LOCK == 0)

    {

    }

    In any case, let me underline that, if you want to change the mode configuration, you can use the graphic interface (section Module Entry of the Clock Component) by enabling the Advanced Mode. 

    Regards,

    Luigi

    sjpatel19922
    Associate II
    March 9, 2017
    Posted on March 09, 2017 at 16:49

    Thanks Luigi, I was able to get it working. Unfortunately, SPC5 studio only seems to be working partially on my computer. I am able to work with the examples that were meant to run on development boards, but I cannot create a project from scratch as it does not show me the configuration options. 

    I have another question related to this.

    What is the input clock source for the System Timer Module? In the datasheet, it mentions the 'System Clock', but it looks like the clock source is IPS_CLK

    Thanks

    zambrano.luigi
    ST Employee
    March 10, 2017
    Posted on March 10, 2017 at 08:30

    Hi,

    about the STM clock, you are right. The counter of the STM is driven by the PBRIDGE (IPS) clock divided by an 8-bit prescale value (1 to 256). There is an error in the Reference Manual that will be correct in the next review. If you give a look to the SPC5Studio example named 'SPC570Sxx_RLA STM Test Application for Discovery', the IPS clock is set to 40MHz, the STM System Clock Prescaler is set to 40 and the counters of the 4 STM0 channels are set to 1000000, 2000000, 3000000 and 4000000. In this way the STM CH0 generates a interrupt after 1 sec, the CH1 after 2 sec, the CH3 after 3 sec and the CH4 after 4 sec.

    Regards,

    Luigi