Skip to main content
Moamen Ayman
Associate III
October 22, 2016
Question

STM32F4 programming

  • October 22, 2016
  • 4 replies
  • 1052 views
Posted on October 22, 2016 at 15:17

Hello, I'm trying to program STM32F407vgt6 chip using IAR and the code works fine but when I disconnect the power and connect it again the chip doesn't work like if the code in the flash memory was deleted and it need to be reprogrammed again to work. I connected Boot0 pin to the ground through 10kOhm resistor and configuring the clock to work at 168MHz from PLL sourced by HSI. could someone tell me what the problem may in?

and thanks in advance.

#clive1 #clive1
    This topic has been closed for replies.

    4 replies

    Tesla DeLorean
    Guru
    October 22, 2016
    Posted on October 22, 2016 at 16:01

    Use the ST-LINK Utilities to confirm if the memory is empty, or still contains exactly what you wrote there.

    Identify all the while() loops your code, and that in the library/startup, might end up in and have those output to a GPIO pin, LED, or USART so you can identify where and how far into your code the system has made it.

    BOOT0 Low should be sufficient to get your code to execute, you'd want to examine BOOT1, and the NRST pin.

    I'd assume that the flash isn't getting erased, and there is some other issue with clocks or code.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    Moamen Ayman
    Associate III
    October 22, 2016
    Posted on October 22, 2016 at 17:58

    yes the problem was in the 10KOhm resistor because it results 1.4V on the BOOT0 pin, when I replaced it with zero ohm resistor it works fine.

    Thanks a lot

    kakaducsy
    Associate
    October 23, 2016
    Posted on October 23, 2016 at 10:56

    Hi clive 1,

    I am communicating with the ps2 using spi dma, but it did not work setup DMA

    void
    DMA_SPI()
    {
    //TX
    DMA_Init_SPI.DMA_Channel = DMA_Channel_3;
    DMA_Init_SPI.DMA_PeripheralBaseAddr = (uint32_t)&(SPI1->DR);
    DMA_Init_SPI.DMA_Memory0BaseAddr = (uint32_t)SPI_Out;
    DMA_Init_SPI.DMA_DIR = DMA_DIR_MemoryToPeripheral;
    DMA_Init_SPI.DMA_BufferSize = 9;
    DMA_Init_SPI.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
    DMA_Init_SPI.DMA_MemoryInc = DMA_MemoryInc_Enable;
    DMA_Init_SPI.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
    DMA_Init_SPI.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;
    DMA_Init_SPI.DMA_Mode = DMA_Mode_Normal;
    DMA_Init_SPI.DMA_Priority = DMA_Priority_Medium;
    DMA_Init_SPI.DMA_FIFOMode = DMA_FIFOMode_Disable;
    DMA_Init_SPI.DMA_FIFOThreshold = DMA_FIFOThreshold_1QuarterFull;
    DMA_Init_SPI.DMA_MemoryBurst = DMA_MemoryBurst_Single;
    DMA_Init_SPI.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
    DMA_Init(DMA2_Stream3, &DMA_Init_SPI);
    NVIC_EnableIRQ(DMA2_Stream3_IRQn);
    DMA_ITConfig(DMA2_Stream3, DMA_IT_TC, ENABLE);
    SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Tx, ENABLE);
    //RX
    DMA_Init_SPI.DMA_Channel = DMA_Channel_3;
    DMA_Init_SPI.DMA_PeripheralBaseAddr = (uint32_t)&(SPI1->DR);
    DMA_Init_SPI.DMA_Memory0BaseAddr = (uint32_t)SPI_In;
    DMA_Init_SPI.DMA_DIR = DMA_DIR_PeripheralToMemory;
    DMA_Init_SPI.DMA_BufferSize = 9;
    DMA_Init_SPI.DMA_PeripheralInc = DMA_PeripheralInc_Disable;
    DMA_Init_SPI.DMA_MemoryInc = DMA_MemoryInc_Enable;
    DMA_Init_SPI.DMA_PeripheralDataSize = DMA_PeripheralDataSize_Byte;
    DMA_Init_SPI.DMA_MemoryDataSize = DMA_MemoryDataSize_Byte;
    DMA_Init_SPI.DMA_Mode = DMA_Mode_Normal;
    DMA_Init_SPI.DMA_Priority = DMA_Priority_Medium;
    DMA_Init_SPI.DMA_FIFOMode = DMA_FIFOMode_Disable;
    DMA_Init_SPI.DMA_FIFOThreshold = DMA_FIFOThreshold_1QuarterFull;
    DMA_Init_SPI.DMA_MemoryBurst = DMA_MemoryBurst_Single;
    DMA_Init_SPI.DMA_PeripheralBurst = DMA_PeripheralBurst_Single;
    DMA_Init(DMA2_Stream0, &DMA_Init_SPI);
    NVIC_EnableIRQ(DMA2_Stream0_IRQn);
    DMA_ITConfig(DMA2_Stream0, DMA_IT_TC, ENABLE);
    SPI_I2S_DMACmd(SPI1, SPI_I2S_DMAReq_Rx, ENABLE);
    }

    set up SPI

    void
    SPI_config()
    {
    SPI_I2S_DeInit(SPI1);
    //configure the SPI
    SPI_InitStructure.SPI_BaudRatePrescaler = SPI_BaudRatePrescaler_256; 
    //8MHz/64 = 125000kHz
    SPI_InitStructure.SPI_CPHA = SPI_CPHA_2Edge; 
    //sample on second edge (falling) of clock
    SPI_InitStructure.SPI_CPOL = SPI_CPOL_High; 
    //clock high when idle
    SPI_InitStructure.SPI_CRCPolynomial = 0;
    SPI_InitStructure.SPI_DataSize = SPI_DataSize_8b; 
    //send 8 bits at a time
    SPI_InitStructure.SPI_Direction = SPI_Direction_2Lines_FullDuplex; 
    //full duplex communication
    SPI_InitStructure.SPI_FirstBit = SPI_FirstBit_LSB; 
    //least significant bit first
    SPI_InitStructure.SPI_NSS = SPI_NSS_Soft;
    SPI_InitStructure.SPI_Mode = SPI_Mode_Master;
    SPI_Init(SPI1, &SPI_InitStructure);
    SPI_Cmd(SPI1, ENABLE);
    }

    interrupt

    //RX
    void
    DMA2_Stream0_IRQHandler(
    void
    )
    {
    if
    (DMA_GetITStatus(DMA2_Stream0, DMA_IT_TCIF0) == SET)
    {
    DMA_ClearITPendingBit(DMA2_Stream0, DMA_IT_TCIF0);
    delay_us(20);
    GPIO_SetBits(GPIOA, GPIO_Pin_4); 
    SPI_work=0;
    i++;
    }
    }
    //-----------------------------------------------------------------
    //TX
    void
    DMA2_Stream3_IRQHandler(
    void
    )
    {
    if
    (DMA_GetITStatus(DMA2_Stream3, DMA_IT_TCIF3) == SET)
    {
    DMA_ClearITPendingBit(DMA2_Stream3, DMA_IT_TCIF3);
    j++;
    }
    }

    start spi

    void
    StartSPI(uint8_t number)
    {
    DMA_SetCurrDataCounter(DMA2_Stream0,number);
    DMA_SetCurrDataCounter(DMA2_Stream3,number);
    SPI_work=1;
    GPIO_ResetBits(GPIOA, GPIO_Pin_4); 
    DMA_Cmd(DMA2_Stream0,ENABLE);
    DMA_Cmd(DMA2_Stream3,ENABLE);
    }

    wait and recieve data

    void
    SPIwait(
    void
    )
    {
    while
    (SPI_work){}
    }
    void
    SetSPI_Out(uint8_t Adr,uint8_t Data)
    {
    if
    (Adr<9)
    {
    SPI_Out[Adr]=Data;
    }
    }
    uint8_t GetSPI_In(uint8_t Adr)
    {
    return
    SPI_In[Adr];
    }

    in main

    int
    main(
    void
    )
    {
    PeriphClk_config();
    GPIO_config();
    Timer3_config();
    SPI_config();
    DMA_SPI();
    //PS2_Send_Recive(PS2,Data, 9);
    SetSPI_Out(0,0x01);
    SetSPI_Out(1,0x42);
    SetSPI_Out(2,0x00);
    SetSPI_Out(3,0x00);
    SetSPI_Out(4,0x00);
    SetSPI_Out(5,0x00);
    SetSPI_Out(6,0x00);
    SetSPI_Out(7,0x00);
    SetSPI_Out(8,0x00);
    StartSPI(9);
    SPIwait();
    while
    (1){}

    when i read data SPI_In i see all value =255,incorrect the value correct is : i send 0x01 : recieve 255 ;0x42--155;0x00--90;0x00--255 help me
    Tesla DeLorean
    Guru
    October 23, 2016
    Posted on October 23, 2016 at 14:51

    This seems off-topic, start a new thread when it is appropriate. There is a ''New'' button in the left corner of the thread list.

    Code doesn't look unreasonable, but is incomplete, you could have just pasted a complete working example. Suggest you get a scope or analyzer and review the signal on the pins. Not clear what you are communicating with, but would suggest you try without DMA first and prove that works/responds as expected.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..