Interfacing with External SPI Flash Memory M25P40
- November 16, 2017
- 0 replies
- 681 views
Hello,
I'm tring to read and write data from a SPI Flash Memory M25P40 with an STM32F103VDT
As first try, I started to read the flash memory serial number.
I used Cube32Mx to generate the initialization code.
This is the SPI3 initialisation function:
static void MX_SPI3_Init(void)
{
hspi3.Instance = SPI3;
hspi3.Init.Mode = SPI_MODE_MASTER;
hspi3.Init.Direction = SPI_DIRECTION_2LINES;
hspi3.Init.DataSize = SPI_DATASIZE_8BIT;
hspi3.Init.CLKPolarity = SPI_POLARITY_LOW;
hspi3.Init.CLKPhase = SPI_PHASE_1EDGE;
hspi3.Init.NSS = SPI_NSS_HARD_OUTPUT;
hspi3.Init.BaudRatePrescaler = SPI_BAUDRATEPRESCALER_8;
hspi3.Init.FirstBit = SPI_FIRSTBIT_MSB;
hspi3.Init.TIMode = SPI_TIMODE_DISABLE;
hspi3.Init.CRCCalculation = SPI_CRCCALCULATION_DISABLE;
hspi3.Init.CRCPolynomial = 10;
if (HAL_SPI_Init(&hspi3) != HAL_OK)
{
_Error_Handler(__FILE__, __LINE__);
}
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
I configure the SPI to use the Interrupt and this is my SPI code:
uint8_t SPI_Read( SPI_Channel_t channel, uint8_t* buffer, uint16_t bufferSize, uint32_t timeout )
{
uint8_t opResult;
opResult = ( HAL_SPI_Receive_IT( SPI_Handlers[channel], buffer, bufferSize ) == HAL_OK ) ? TRUE : FALSE;
opResult &= (osSemaphoreWait( SPI_RX_SemaphoreId[channel], timeout ) == osOK ? TRUE : FALSE );
return opResult;
}
uint8_t SPI_Write( SPI_Channel_t channel, uint8_t* buffer, uint16_t bufferSize, uint32_t timeout )
{
uint8_t opResult;
opResult = ( HAL_SPI_Transmit_IT(SPI_Handlers[channel], buffer, bufferSize) == HAL_OK ) ? TRUE : FALSE;
opResult &= ( osSemaphoreWait( SPI_TX_SemaphoreId[channel], timeout ) == osOK ? TRUE : FALSE );
return opResult;
}
uint8_t SPI_WriteRead( SPI_Channel_t channel, uint8_t* bufferIn, OUT uint8_t* bufferOut, uint16_t bufferSize, uint32_t timeout )
{
uint8_t opResult;
opResult = ( HAL_SPI_TransmitReceive_IT(SPI_Handlers[channel], bufferIn, bufferOut, bufferSize) == HAL_OK ) ? TRUE : FALSE;
opResult &= ( osSemaphoreWait( SPI_TXRX_SemaphoreId[channel], timeout ) == HAL_OK ? TRUE : FALSE );
return opResult;
}
/*========== Interrupt callback ==========*/
void HAL_SPI_TxCpltCallback(SPI_HandleTypeDef *hspi)
{
SPI_Channel_t channel;
if( hspi == SPI_Handlers[SPI_BLUETOOTH] ) { channel = SPI_BLUETOOTH; }
else if( hspi == SPI_Handlers[SPI_EFLASH] ) { channel = SPI_EFLASH; }
else
{
/* TODO: error */
LOG_Print( LOG_SOURCE_SPI, LOG_LEVEL_ERROR, ''[SPI] Tx cb unknown channel'');
return;
}
osSemaphoreRelease( SPI_TX_SemaphoreId[channel] );
}
void HAL_SPI_RxCpltCallback(SPI_HandleTypeDef *hspi)
{
SPI_Channel_t channel;
if( hspi == SPI_Handlers[SPI_BLUETOOTH] ) { channel = SPI_BLUETOOTH; }
else if( hspi == SPI_Handlers[SPI_EFLASH] ) { channel = SPI_EFLASH; }
else
{
/* TODO: error */
LOG_Print( LOG_SOURCE_SPI, LOG_LEVEL_ERROR, ''[SPI] Rx cb unknown channel'');
return;
}
osSemaphoreRelease( SPI_RX_SemaphoreId[channel] );
}
void HAL_SPI_TxRxCpltCallback(SPI_HandleTypeDef *hspi)
{
SPI_Channel_t channel;
if( hspi == SPI_Handlers[SPI_BLUETOOTH] ) { channel = SPI_BLUETOOTH; }
else if( hspi == SPI_Handlers[SPI_EFLASH] ) { channel = SPI_EFLASH; }
else
{
/* TODO: error */
LOG_Print( LOG_SOURCE_SPI, LOG_LEVEL_ERROR, ''[SPI] TxRx cb unknown channel'');
return;
}
osSemaphoreRelease( SPI_TXRX_SemaphoreId[channel]);
}�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?�?
As you can see in the above code, the semaphore is released by the Tx/Rx/TxRx interrupt.
When I try to perform a simple serial number read, the Rx Interrupt is not raised.
This is the code to read the flash memory serial number:
opResult = SPI_Write( SPI_EFLASH, 0x9F, 1, EFLASH_WRITE_COMMAND_TIMEOUT );
/* The serial number has 20 bytes */
opResult = SPI_Read( SPI_EFLASH, buffer, 20, EFLASH_READ_COMMAND_TIMEOUT );�?�?�?�?
Unfortunately, the read operation fails dut to semaphore timeout. This happens because the Rx interrupt is not raised.
I also the SPI communication with a logic analyzer and the serial number bytes are exchanged on the SPI ad you can see in the below image:
Any suggestion?
I checked everything... But maybe I forget something.
Thanks!
#spi-write-and-read #flash-memory #stm32f1-spi