Associate II
March 8, 2017
Solved
CubeMX problem (bug?)
- March 8, 2017
- 7 replies
- 2438 views
Posted on March 08, 2017 at 14:33
Hi,
I'm having problems with STM32 CubeMX (v4.19.0) during the setup of the ADC2 peripheral (may be a bug...).
Even if the number of conversion is ONE, I have two different ranks both pointing to the same ADC channel (please refer to the attached screenshot).
I looked into the ioc and some lines don't convince me (I have only channel 4 active):
'...
ADC2.Channel-20\&sharpChannelRegularConversion=ADC_CHANNEL_4
ADC2.Channel-4\&sharpChannelRegularConversion=ADC_CHANNEL_4ADC2.Channel-8\&sharpChannelRegularConversion=ADC_CHANNEL_4...'
Is there any .ioc file cleaner that can fix this behavior?
Thanks in advance
Flavio
#cubemx-bug