Skip to main content
piotr239955_st
Associate II
May 3, 2017
Question

STM32F030K6 start only with reset tie to VCC

  • May 3, 2017
  • 8 replies
  • 2080 views
Posted on May 03, 2017 at 19:18

I have device with STM32f030K6T6. Since one moment, I am not able to start this uP without shorcircuiting nReset signal to VCC. Originally I had RC circuit on this line. When this problem had occured I modified it removing resistor (leaving capacitor connected between nReset and GND). Still doesn't work. Currently I'm running very simple program with for(;;) loop.

Main question is: what kind of setting may cause that? At some point I was using settings in ST-Link with 'Program under reset', but now I change that to 'normal & autodetect' but behavior is still the same.

Note: this post was migrated and contained many threaded conversations, some content may be missing.
    This topic has been closed for replies.

    8 replies

    Tesla DeLorean
    Guru
    May 3, 2017
    Posted on May 03, 2017 at 19:23

    I would guess you don't have VDDA wired up properly to a supply.

    Short circuiting the pin suggests come chronic design failure on your end.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
    piotr239955_st
    Associate II
    May 3, 2017
    Posted on May 03, 2017 at 19:29

    VDDA is connectected directly to VCC and 100nF capacitor is placed as close as possible.

    Tesla DeLorean
    Guru
    May 3, 2017
    Posted on May 03, 2017 at 19:38

    If the supply is below threshold on VDDA the device will have NRST clamped internally.

    If NRST with a pull-up is LOW, something in the circuit is driving it there or clamping. The STM32 won't naturally do that. You need to look critically at the circuits on the board, review the netlist carefully. Measure the voltage on VDDA.

    Double check pin list against datasheet, and that part is correctly orientated.

    Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..