Skip to main content
jampino
Associate III
July 9, 2018
Question

Bluenrg-1 DTM failing

  • July 9, 2018
  • 1 reply
  • 617 views
Posted on July 09, 2018 at 14:13

Hello all,

I am using the DTM for bluenrg-1 I can program the unit and it will work fine but for some reason when the unit is left powered down for a couple of hours and then powered up again some times stops working.

Doing a flash reading starting in address 0x

10040000

I can see the next difference:

On the unit that is working:

00

60

00 20 61 16 04 10 29 18 04 10 39 18 04 10

On the unit that stops working:

00

00

00 20 61 16 04 10 29 18 04 10 39 18 04 10

For some reason that byte changes value.

Any idea why that problem could happen.

Thank you

    This topic has been closed for replies.

    1 reply

    jampino
    jampinoAuthor
    Associate III
    September 14, 2018

    I have seen a different problem, the bluenrg-1 was working fine pairing and communicating with other devices, then I powered down for a time and next time I power up the unit didn't work.

    Reading some locations from flash I can see that they are 0xff somehow the flash got corrupted/blank.

    Someone has seen that problem before.

    Thank you