Skip to main content
Vu.Andy
Associate III
November 15, 2017
Solved

HAL_PWR_EnterSTANDBYMode() does not put uC into sleep mode.

  • November 15, 2017
  • 2 replies
  • 3012 views
Posted on November 15, 2017 at 19:54

I am using STM32F042F6 uC.  I am not sure why this HAL_PWR_EnterSTANDBYMode() does not put the uC to sleep mode.  But the odd thing is in certain condition, it does go the Standby mode, but in some other boards, the uC does not go to standby mode. 

I would think this function is unconditionally put the uC to Standby mode.  Is there any condition in which the uC cannot be put into Standby mode?  Why would in some condition I can put uC in standby and in some I could not?

Thanks.

This topic has been closed for replies.
Best answer by Nesrine M_O
Posted on November 16, 2017 at 14:04

Hi

Vu.Andy

,

I recommend you to start from ready example under the

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef0.html

firmware package:

STM32Cube_FW_F0_V1.9.0\Projects\STM32072B_EVAL\Examples\PWR\PWR_STANDBY

-Nesrine-

2 replies

Nesrine M_O
Nesrine M_OBest answer
Associate
November 16, 2017
Posted on November 16, 2017 at 14:04

Hi

Vu.Andy

,

I recommend you to start from ready example under the

http://www.st.com/content/st_com/en/products/embedded-software/mcus-embedded-software/stm32-embedded-software/stm32cube-embedded-software/stm32cubef0.html

firmware package:

STM32Cube_FW_F0_V1.9.0\Projects\STM32072B_EVAL\Examples\PWR\PWR_STANDBY

-Nesrine-

Vu.Andy
Vu.AndyAuthor
Associate III
November 16, 2017
Posted on November 16, 2017 at 20:07

 ,

 ,

Thank you.

After looking into the example, apparently I have to execute the following codes before going into standby mode.

I am using the IWDG to wake up so the Wakeup in is not needed.

 , __HAL_RCC_PWR_CLK_ENABLE(), , , ,

 , /* ♯ ♯ ♯ ♯ Disable all used wakeup sources: WKUP pin ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */

 ,

 , HAL_PWR_DisableWakeUpPin(PWR_WAKEUP_PIN1),

 ,

 ,

 ,

 , /* ♯ ♯ ♯ ♯ Clear all related wakeup flags ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ ♯ */

 ,

 , /* Clear PWR wake up Flag */

 ,

 , __HAL_PWR_CLEAR_FLAG(PWR_FLAG_WU),

 ,

 ,

 ,

 , /* Disable WKUP pin */

 ,

// , HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN2),

 ,

 , ,  ,

 ,

 , ,  ,HAL_PWR_EnterSTANDBYMode(),