Skip to main content
pontus2
Associate II
June 28, 2016
Question

Trouble connecting to AP (using WPA2)

  • June 28, 2016
  • 1 reply
  • 564 views
Posted on June 28, 2016 at 16:25

I am trying to connect my SPWF01S to an AP but am not able to do so. This is the WINDS i get:

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete (0x0)

+WIND:19:WiFi Join:74:EA:3A:D3:C4:D4

+WIND:25:WiFi Association with 'InOutDemo' successful

+WIND:40:WiFi Deauthentication:2

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete (0x0)

+WIND:74:Rejected found Network

+WIND:74:Rejected found Network

+WIND:21:WiFi Scanning

+WIND:35:WiFi Scan Complete (0x0)

+WIND:74:Rejected found Network

And this is the config:

# Dumping All Configuration Keys:

#  nv_manuf = ST

#  nv_model = SPWF01S

#  nv_serial = value

#  nv_wifi_macaddr = 00:80:E1:B8:33:20

#  etf_mode = 0

#  blink_led = 0

#  wind_off_low = 0x00000000

#  wind_off_medium = 0x00000000

#  wind_off_high = 0x00000000

#  user_desc = anonymous

#  escape_seq = at+s.

#  localecho1 = 0

#  console1_speed = 115200

#  console1_hwfc = 0

#  console1_enabled = 1

#  console1_delimiter = 0x0000002C

#  console1_errs = 1

#  sleep_enabled = 0

#  standby_enabled = 0

#  standby_time = 10

#  wifi_tx_msdu_lifetime = 0

#  wifi_rx_msdu_lifetime = 0

#  wifi_operational_mode = 0x00000011

#  wifi_beacon_wakeup = 1

#  wifi_beacon_interval = 100

#  wifi_listen_interval = 0

#  wifi_rts_threshold = 3000

#  wifi_ssid = 49:6E:4F:75:74:44:65:6D:6F:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_ssid_len = 9

#  wifi_txfail_thresh = 5

#  wifi_ht_mode = 0

#  wifi_channelnum = 6

#  wifi_opr_rate_mask = 0x00003FCF

#  wifi_bas_rate_mask = 0x0000000F

#  wifi_mode = 1

#  wifi_region = 1

#  wifi_auth_type = 0

#  wifi_atim_window = 0

#  wifi_powersave = 0

#  wifi_tx_power = 18

#  wifi_rssi_thresh = 0

#  wifi_rssi_hyst = 0

#  wifi_ap_idle_timeout = 120

#  wifi_beacon_loss_thresh = 10

#  wifi_priv_mode = 2

#  wifi_wep_keys[0] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[1] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[2] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_keys[3] = 00:00:00:00:00:00:00:00:00:00:00:00:00:00:00:00

#  wifi_wep_key_lens = 00:00:00:00

#  wifi_wep_default_key = 0

#  wifi_wpa_psk_raw = 5D:50:2E:22:88:13:4B:65:CE:8A:03:E2:CF:4E:8C:64:20:69:34:83:6B:F3:0D:C2:92:1B:15:C5:0A:22:87:6E

#  wifi_wpa_psk_text =  inoutserverdemo

#  ip_use_dhcp = 1

#  ip_use_httpd = 1

#  ip_mtu = 1500

#  ip_hostname = iwm-B8-33-20

#  ip_apdomainname = captiveportal.net

#  ip_apredirect = firstset.html

#  ip_ipaddr = 192.168.0.50

#  ip_netmask = 255.255.255.0

#  ip_gw = 192.168.0.1

#  ip_dns = 192.168.0.1

#  ip_http_get_recv_timeout = 3000

#  ip_wait_timeout = 12000

#  ip_dhcp_timeout = 20

#  ip_sockd_timeout = 250

#  ip_dhcp_lease_time = 120

#  ip_dns_mode = 0

#  ip_use_cgis = 0x0000000F

#  ip_use_ssis = 0x0000000F

#  ip_use_decoder = 0x00000000

    This topic has been closed for replies.

    1 reply

    Gerardo GALLUCCI
    ST Employee
    July 4, 2016
    Posted on July 04, 2016 at 11:18

    Can you also share AP details? b/g/n, authentication type, PSK, etc...

    Deauthentication reason 2 means:

    Code-2

     

    prior authentication is not valid

    Regards

    jerry