Skip to main content
Konami
Senior
February 26, 2018
Solved

Nucleo64 Power Measurement

  • February 26, 2018
  • 14 replies
  • 2062 views
Posted on February 26, 2018 at 17:34

I'm measuring the current on JP6 (IDD) and I see 4mA at the lowest when running the Power_Management sample or even holding the MCU in reset. I am powering the board via the USB connector. Is this incorrect?

I've tried using SLEEP_MODE, STANDBY_MODE, and STOP_MODE defined, and they all show around 4mA

Nucleo-F411RE

    This topic has been closed for replies.
    Best answer by Bogdan Golab
    Posted on February 26, 2018 at 18:53

    Look at the table 26 (I guess we are talking about Sleep Mode), check the frequency to see if what you see is far from what is expected:

    http://www.st.com/content/ccc/resource/technical/document/datasheet/b3/a5/46/3b/b4/e5/4c/85/DM00115249.pdf/files/DM00115249.pdf/jcr:content/translations/en.DM00115249.pdf

     

    14 replies

    Andrew Neil
    Super User
    February 26, 2018
    Posted on February 26, 2018 at 17:37

    Have you disconnected everything else from the microcontroller - ST-Link, LEDs, Buttons, etc, etc, ... ?

    See:

    https://community.st.com/0D50X00009XkWhGSAV

    - and follow the links ,,,

    A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
    Konami
    KonamiAuthor
    Senior
    February 26, 2018
    Posted on February 26, 2018 at 18:55

    No I haven't disconnected anything. The user manual for the board indicates that simply measuring IDD should give the STM32 current  consumption. Do I need to remove components? That seems like a really ineffective feature if that's the case.

    http://www.st.com/content/ccc/resource/technical/document/user_manual/98/2e/fa/4b/e0/82/43/b7/DM00105823.pdf/files/DM00105823.pdf/jcr:content/translations/en.DM00105823.pdf

     
    Bogdan Golab
    Lead
    February 26, 2018
    Posted on February 26, 2018 at 18:09

    VDD is used only for target MCU.

    ST-LINK uses 3.3V directly - VDD is delivered through the JP6. So it seems that the ST-LINK current is not counted into total current consuption.

    Button uses pull-up resistor (when pressed 3.3V/4.7k =0.7mA ) and LED ((3.3-1.6)/0.51k = 3.3mA) if enabled adds its current. I believe that the LED is off during the test and the button was not pressed.

    Not sure what board you use to see the relevant datasheet data

    Bogdan Golab
    Lead
    February 26, 2018