Skip to main content
astrid
Associate II
November 25, 2015
Question

STM32F1 PWM wit DMA?

  • November 25, 2015
  • 2 replies
  • 735 views
Posted on November 26, 2015 at 00:46

Můžete zadat text �?i webovou adresu nebo

https://translate.google.cz/?tr=f&hl=cs

.

https://translate.google.cz/?tr=t&hl=cs

</div>

Zobrazuje se překlad pro text

Přeložit raději text

If

I understand

correctly, the function

HAL_TIM_PWM_Start_DMA(TIM_HandleTypeDef *htim, uint32_t Channel, uint32_t *pData, uint16_t Length)

Start PWM and over DMA transfer data from  pData to CCR1 register of Timer.

If I''m true and CCR1 is 16bit register why is pData pointer on

uint32_t

?

How use it with for example uint16_t Buffer[1000];?

    This topic has been closed for replies.

    2 replies

    Nickname5522_O
    Visitor II
    November 26, 2015
    Posted on November 26, 2015 at 18:10

    Himark.aster,

    If you have a look to the definition of the register CC1 under stm32f1*.h, you will find that it is declared of type uint32_t

    __IO uint32_t CCR1; /*!< TIM capture/compare register 1, Address offset: 0x34 */

    The fact that CCR1 is a 16 bit register is not contradictory with declaring it as uint32_t . The goal is to keep the code homogeneous. By consequence, if you want to use an uint16_t buffer, you must change all related variables and parameters in the HAL library, which is not obvious. -Shahrzad-
    astrid
    astridAuthor
    Associate II
    November 26, 2015
    Posted on November 26, 2015 at 21:50

    Thank you for answer

    .