Skip to main content
Associate II
Nov 10, 2015 9:24 PM UTC
Question

HAL UART PROBLEM ON F103CB

Posted on November 10, 2015 at 22:24

The original post was too long to process during our migration. Please click on the attachment to read the original post.
    This topic has been closed for replies.

    1 reply

    nima2Author
    Associate II
    Nov 13, 2015 3:22 PM UTC
    Posted on November 13, 2015 at 16:22

    I changed my code to:

    void InitUsart(void) {
    __GPIOA_CLK_ENABLE();
    /**USART2 GPIO Configuration
    PA2 ------> USART2_TX
    PA3 ------> USART2_RX
    */
    GPIO_InitStruct.Pin = GPIO_PIN_2 | GPIO_PIN_3;
    GPIO_InitStruct.Mode = GPIO_MODE_AF_PP;
    GPIO_InitStruct.Pull = GPIO_NOPULL;
    GPIO_InitStruct.Speed = GPIO_SPEED_LOW;
    HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);
    __USART2_CLK_ENABLE();
    UartHandle.Instance = USART2;
    UartHandle.Init.BaudRate = 115200;
    UartHandle.Init.WordLength = UART_WORDLENGTH_8B;
    UartHandle.Init.StopBits = UART_STOPBITS_1;
    UartHandle.Init.Parity = UART_PARITY_NONE;
    UartHandle.Init.HwFlowCtl = UART_HWCONTROL_NONE;
    UartHandle.Init.Mode = UART_MODE_TX_RX;
    if (HAL_UART_Init(&UartHandle) != HAL_OK) {
    /* Initialization Error */
    // Error_Handler();
    }
    if (HAL_UART_Transmit(&UartHandle, (uint8_t *) ''TEST'', 4,
    5000) != HAL_OK) {
    /* Transfer error in transmission process */
    //Error_Handler();
    }
    }

    and it works fine but I can just send data and still I could not receive data with this code:

    HAL_UART_Receive(&UartHandle,(uint8_t *) aRxBuffer, RXBUFFERSIZE, 1000);

    always I get time out error(0x03) please help me :(