Skip to main content
robertnoble9
Associate III
April 7, 2018
Solved

STM32H743 Nucleo DMA transfer error

  • April 7, 2018
  • 2 replies
  • 1756 views
Posted on April 07, 2018 at 15:15

Hi all,

To start with:

Board: STM32H743ZI Nucleo

IDE: Attolic TrueSTUDIO for STM32 9.0.0

HAL version: STM32Cube_FW_H7_V1.2.0

I'm trying to trigger a DMA transfer on DMA1_Stream7 using TIMER 3 CC3.  I want to trigger a transfer from a variable into the CCR for TIM3 channel 3.

I can initial the DMA stream to the configuration I think it should be in but as soon as the stream is enabled I get a transfer error and I can't work out what the problem is.

Any help would be great.

Thanks

Below is a screenshot of DMA1, stream 7 register values.

0690X0000060AH8QAM.png

Below is my DMA stream initialisation code:

void setUpDMA(TIM_HandleTypeDef *htim)

{

static DMA_HandleTypeDef hdma_tim;

/* Enable DMA clock */

__HAL_RCC_DMA1_CLK_ENABLE();

/* Set the parameters to be configured */

hdma_tim.Init.Request = DMA_REQUEST_TIM3_CH3;

hdma_tim.Init.Direction = DMA_MEMORY_TO_PERIPH;

hdma_tim.Init.PeriphInc = DMA_PINC_DISABLE;

hdma_tim.Init.MemInc = DMA_MINC_DISABLE;

hdma_tim.Init.PeriphDataAlignment = DMA_PDATAALIGN_HALFWORD;

hdma_tim.Init.MemDataAlignment = DMA_MDATAALIGN_HALFWORD;

hdma_tim.Init.Mode = DMA_CIRCULAR;

hdma_tim.Init.Priority = DMA_PRIORITY_HIGH;

hdma_tim.Init.FIFOMode = DMA_FIFOMODE_DISABLE;

hdma_tim.Init.FIFOThreshold = DMA_FIFO_THRESHOLD_FULL;

hdma_tim.Init.MemBurst = DMA_MBURST_SINGLE;

hdma_tim.Init.PeriphBurst = DMA_PBURST_SINGLE;

/* Set hdma_tim instance */

hdma_tim.Instance = DMA1_Stream7;

/* Link hdma_tim to hdma[TIM_DMA_ID_CC3] (channel3) */

__HAL_LINKDMA(htim, hdma[TIM_DMA_ID_CC3], hdma_tim);

DMA1->LIFCR = 0xFFFF;

DMA1->HIFCR = 0xFFFF;

/* Initialize TIMx DMA handle */

HAL_DMA_Init(htim->hdma[TIM_DMA_ID_CC3]);

}

UPDATE:  SOLVED

As JW pointed out, the memory address of the variable I was trying to transfer was in TCM memory, which DMA1 and DMA2 do not have access to.  After adding __attribute__((section(''.sram_d2'')) to the definition of the variable, it was placed into SRAM in domain 2 (address 0x30000000),  this solved the problem (YAY).

    This topic has been closed for replies.
    Best answer by waclawek.jan
    Posted on April 09, 2018 at 21:08

    The DTCM-RAM is available only to the processor and MDMA. Use other RAM (preferrably one of those in the D2 domain).

    JW

    2 replies

    waclawek.jan
    waclawek.janBest answer
    Super User
    April 9, 2018
    Posted on April 09, 2018 at 21:08

    The DTCM-RAM is available only to the processor and MDMA. Use other RAM (preferrably one of those in the D2 domain).

    JW

    Felipe Navarro
    Associate
    April 10, 2018
    Posted on April 10, 2018 at 04:38

    Take a look into this thread, at least for the ADC it helped with my problem:

    https://community.st.com/0D50X00009XkXEHSA3