Question
Calculation Adc value based on CubeMx
Posted on March 16, 2016 at 02:42
Hello guys.
I am using STM32F051K8 with CubeMX. While using ADC conversion, the adc value is working weird.The value I measured is adc value from position sensor. the range is from 0 to 2.9V(measured with Oscilloscope).When the value is reached in 2.9v, the measured ad value is 3600 which is correct(3600/4095 * 3.3v). However the ad value became 0 when it measured below than 0.7v.Is there any calculation that I missed?For example, if 1v is measured, I think the ad value should be 1240 (1v/3.3v*4095(12bits)) but the real ad value is 280.Please help me with this. Thank you for reading guys. #adc #stm32cube #bug