Skip to main content
baycanakcay
Associate II
March 8, 2018
Question

Low Speed Bldc 6STep Library

  • March 8, 2018
  • 1 reply
  • 578 views
Posted on March 08, 2018 at 10:10

Hi

I am using IHM08M1 board with stm32f302, to drive a bldc 36 volts BLDC motor. I am using SixSTep library (SPN8). 

I need very low speed in my project like 1 rpm. The motor has a 100:1 reduction gear. The minimum speed I got with Sixstep library is 300 rpm. If I set target speed below 300 rpm, motor stops or became unstable. Is there any way to achieve 100 rpm speed, with some modification in the library. I am driving motor in sensorless configuration, the motor have hall sensors, but the library does not include any hall sensor interface Is there any other version of sixstep library with hall sensor interface?

Best regards.

#spn8 #low-rpm-bldc-drive #hall-sensor #6step-library
This topic has been closed for replies.

1 reply

Vitaliy Chernobay
Senior
April 9, 2018
Posted on April 09, 2018 at 18:01

Try PID control?