Associate III
Apr 21, 2017 6:49 PM UTC
Question
STM32CubeMx 4.20.1: Clock Configuration GUI not working
- 9 replies
- 2560 views
Posted on April 21, 2017 at 20:49
Hi all!
The Clock Configuration GUI shows a weird behavior: I'm not able to put a valid input frequency for HSE (or LSE).
For example I want to setup the input frequency to 8 MHz:
- entered value 8 is not accepted - changed to 0.0000000000080 immediately

- entered value 8000000 is accepted and changed to value 8 but as soon as the focus is changed to an other element the value jumps to 0.0000080

Development environment:
- Eclipse Neon 3
- STM32CubeMx version: 4.20.1 (Eclipse plugin)
- Java: jdk1.8.0_25
- ioc config file attached
Best regards,
Michael.