Skip to main content
tanim330
Visitor II
November 23, 2015
Question

STm32L151 temperature sensor example

  • November 23, 2015
  • 0 replies
  • 609 views
Posted on November 23, 2015 at 14:57

I am new to STm32 architecture. Trying  to get the internal temperature sensor going. I am using a STm32L151VC microcontroller, STM32-QFP100 programmer adapter and IAR tool chain. I am trying to use the following code, but looks like ADC conversion is giving me some random value. Sometimes, it shows a random number between 600~700 ( which doesn't make sense as the hot calibration voltage is 626 at 100 degrees according to the data sheet), and the most other time variable AD_value shows 0. Any help/comment will be highly appreciated.

int main(void)

{

 

/* Configure PB.12 (ADC1 Channel18) or PF.10 (ADC1 Channel31) in analog mode -*/

  GPIO_InitStructure.GPIO_Mode  = GPIO_Mode_AN;

  GPIO_InitStructure.GPIO_PuPd  = GPIO_PuPd_NOPULL;

/* Enable the GPIOB Clock */

  RCC_AHBPeriphClockCmd(RCC_AHBPeriph_GPIOB, ENABLE);

  GPIO_InitStructure.GPIO_Pin = GPIO_Pin_12;

  GPIO_Init(GPIOB, &GPIO_InitStructure);  

/* Enable the HSI */

  RCC_HSICmd(ENABLE);

  /* Wait until HSI oscillator is ready */

  while(RCC_GetFlagStatus(RCC_FLAG_HSIRDY) == RESET);

/* ADC1 Configuration -----------------------------------------------------*/

  ADC_InitStructure.ADC_Resolution = ADC_Resolution_12b;

  ADC_InitStructure.ADC_ScanConvMode = ENABLE;

  ADC_InitStructure.ADC_ContinuousConvMode = ENABLE;

  ADC_InitStructure.ADC_ExternalTrigConvEdge = ADC_ExternalTrigConvEdge_None;

  ADC_InitStructure.ADC_DataAlign = ADC_DataAlign_Right;

  ADC_InitStructure.ADC_NbrOfConversion = 1;             // Set conversion data alignement

  ADC_Init(ADC1, &ADC_InitStructure);

 

  ADC_TempSensorVrefintCmd(ENABLE);

 /* Wait until ADC + Temp sensor start */

  T_StartupTimeDelay = 1024;

  while (T_StartupTimeDelay--);

 

 /* Setup ADC common init struct */

  ADC_CommonInitStructure.ADC_Prescaler = ADC_Prescaler_Div4;

  ADC_CommonInit(&ADC_CommonInitStructure);

 

ADC_RegularChannelConfig(ADC1, ADC_Channel_16, 1, ADC_SampleTime_384Cycles);

   

 /* Start ADC1 Software Conversion */

  while (1)

  {

    RCC_APB2PeriphClockCmd(RCC_APB2Periph_ADC1, ENABLE);

  ADC_Cmd(ADC1, ENABLE);

  /* Wait until the ADC1 is ready */

  while(ADC_GetFlagStatus(ADC1, ADC_FLAG_ADONS) == RESET);

  ADC_SoftwareStartConv(ADC1);

  AD_value=ADC_GetConversionValue(ADC1);

 

 

  }

} 
    This topic has been closed for replies.