Skip to main content
trenton
Visitor II
March 28, 2016
Question

STM32F407G-DISC1 requires PC connection to boot

  • March 28, 2016
  • 4 replies
  • 1105 views
Posted on March 28, 2016 at 23:29

Recently the STM32F407 discovery board changed part numbers from STM32F4DISCOVERY to STM32F407G-DISC1. The old boards could be powered directly via the 5V pins on the headers, or via a USB wall-wart, but the new boards need to be connected to a PC in order to boot. Is this intended behavior? Is there a solution aside from flashing an older firmware to the STLink chip?

Thanks

#stm32f407g-disc1
This topic has been closed for replies.

4 replies

Tesla DeLorean
Guru
March 28, 2016
Posted on March 29, 2016 at 00:59

I think it has been discussed or documented. I don't think you can get the older model firmware on the ST-LINK easily.

Check SB11 (NRST)

http://www.st.com/st-web-ui/static/active/en/resource/technical/document/user_manual/DM00039084.pdf

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Walid FTITI_O
Visitor II
April 5, 2016
Posted on April 05, 2016 at 19:18

Hi trent,

You should upgrade your ST-LINK firmware to ST-LINK/V2-1 through

http://www.st.com/web/en/catalog/tools/PF260217

.

-Hannibal-

Recently the STM32F407 discovery board changed part numbers from STM32F4DISCOVERY to STM32F407G-DISC1. The old boards could be powered directly via the 5V pins on the headers, or via a USB wall-wart, but the new boards need to be connected to a PC in order to boot. Is this intended behavior? Is there a solution aside from flashing an older firmware to the STLink chip?

Thanks
NEIL HENRY
Associate II
November 10, 2017
174981CGIL2
Tesla DeLorean
Guru
November 10, 2017
Posted on November 10, 2017 at 22:05

You have a different issue from the one reported by the OP

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..