Question
Select ADC channel to convert
Posted on April 30, 2018 at 18:16
hi, I have a problem using an ADC of a STM32L4
In my project I have to sample 5 analogue channels with an ADC. I've configured everything with STM32CubeMX and want to use it in polling mode. I have seen examples where this code is:HAL_ADC_Start(&hadc);
if (HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY) == HAL_OK) { ADC_ch0_value = HAL_ADC_GetValue(&hadc); HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY); ADC_ch1_value = HAL_ADC_GetValue(&hadc); HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY); ADC_ch2_value = HAL_ADC_GetValue(&hadc); ......}HAL_ADC_Stop(&hadc);in which the channels are converted sequentially, what I would like to do instead is to convert only the selected channel, for example:
HAL_ADC_Start(&hadc);
---> SELECT ADC CHANNEL 3 <---if (HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY) == HAL_OK) { ADC_ch3_value = HAL_ADC_GetValue(&hadc);}HAL_ADC_Stop(&hadc);// other code// other function HAL_ADC_Start(&hadc);---> SELECT ADC CHANNEL 1 <---if (HAL_ADC_PollForConversion(&hadc, HAL_MAX_DELAY) == HAL_OK) { ADC_ch1_value = HAL_ADC_GetValue(&hadc);}HAL_ADC_Stop(&hadc);what I do not know how to do is the code for:
---> SELECT ADC CHANNEL n <---
How can I do? can someone help me?