Override HAL Ethernet Initialisation
Hi,
I am having some issues with the Cube generated Ethernet startup code. I suspect I am discovering limitations in the generated code because of assumptions Cube is making of my hardware.
For reference my setup is as follows:
MCU: STM32F427ZITx on a custom made PCBCube: STM32Cube FW_F4 V1.13.1IDE: System Workbench V1.11.0.201610101240PHY: MICREL KSZ8863MLL Integrated 3-Port 10/100 Managed Switch with 2 PHYsAccess to PHY control registers using MIIMThe issues I am faced with include:
1. Cube assumes I have a single PHY. In my instance I need to configure 2 PHY. This involves modifying the HAL Ethernet driver. There are no user blocks so I'm unsure how to make the necessary changes.2. Cube assumes I can perform certain functions on the PHY. For example, it assumes I can do a soft reset using register 0. This is not supported on my PHY. Performing a reset overrides the register defaults and put the PHY into an unexpected state.3. Cube assumes I have access to the extended registers. The MIIM interface gives me limited access to registers. If I enable auto-negotiation, the last step of Ethernet initialisation in the HAL driver is to read back the Ethernet speed and duplex. Since I can't access the extended registers, the resulting values to the read call (which passes) is 0xFF. Further processing on the value read back results in unintended behavior.My question is, how do I modify the HAL Ether initialisation routine? These best way forward I can see so far is to take a copy of the generated code I have so far, turn of Cube code generation for the Ethernet interface, copy the code back into my project and modify it to suit. Is this how I should proceed?
Regards, Matt.
#ksz8863 #hal_eth_init #micrel