Skip to main content
swarnkarankit47
Associate II
June 8, 2018
Question

Debug Port Fail in SPC5xx

  • June 8, 2018
  • 2 replies
  • 1063 views
Posted on June 08, 2018 at 07:14

I am working on SPC563M64 controller. I have started working on shadow flash now. But during testing of shadow flash code I got debug port fail error while trying to connect to controller. I think the board is permanently reset and I am not able to connect to my board again. What can I do ? I have also tried the sequence of commands in a sequence listed below but still I was not able to connect to controller :

1. system.option.cpu   

2.SYStem.Option.KEYCODE 0xFEEDFACECAFEBEEF

3. system.up.

Please tell me what is this issue is ?

#spc5x
    This topic has been closed for replies.

    2 replies

    Erwan YVIN
    ST Technical Moderator
    June 8, 2018
    Posted on June 08, 2018 at 09:59

    Hello Ankit ,

    You are using TRACE32 lautechbach ..

    Have you updated the shadow flash ?

    could you try to click on Reset Button of your board in trying to connect the debugger in the same time .

    Maybe , there is a sort of reset escalation.

         Best Regards

                          Erwan

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
    swarnkarankit47
    Associate II
    June 8, 2018
    Posted on June 08, 2018 at 10:31

    Yes I updated shadow flash and after that I did reset and from then this problem is coming.

    I tried to connect to board while press the reset button at the same time but error showed that ' target reset failed '.