Skip to main content
GreenGuy
Senior III
March 30, 2018
Solved

error: array type has incomplete element type

  • March 30, 2018
  • 5 replies
  • 3356 views
Posted on March 30, 2018 at 07:29

This is occurring in fsdata_custom.c in the LwIP_HTTP_Server_Netconn_RTOS project I imported from CubeMX.  The struct that is being referenced is :

struct fsdata_file {

  const struct fsdata_file *next;

  const unsigned char *name;

  const unsigned char *data;

  int len;

  u8_t flags;

#if HTTPD_PRECALCULATED_CHECKSUM

  u16_t chksum_count;

  const struct fsdata_chksum *chksum;

#endif /* HTTPD_PRECALCULATED_CHECKSUM */

};

and the HTTPD_PRECALCULATED_CHECKSUM is defined as 0.

Where the error is occurring in fsdata_custom.c is at: (line 2336

const struct fsdata_file file__STM32F7xx_files_logo_jpg[] = { {

file_NULL,

data__STM32F7xx_files_logo_jpg,

data__STM32F7xx_files_logo_jpg + 28,

sizeof(data__STM32F7xx_files_logo_jpg) - 28,

1,

}};

According to the struct definition it looks like all the elements are there so I am confused.

Anyone run across this?

    This topic has been closed for replies.
    Best answer by Ben S
    Posted on June 28, 2018 at 07:00

    In case anyone else comes across this - fsdata_custom.c isn't meant to be directly compiled, it gets included in httpd/fs.c.  I removed fsdata_custom.c from my Makefile and the errors went away

    5 replies

    Ben S
    Associate
    June 27, 2018
    Posted on June 27, 2018 at 20:31

    hey greg - did you ever find a solution to this?  I'm having the same problem and can't seem to figure it out

    Ben S
    Ben SBest answer
    Associate
    June 28, 2018
    Posted on June 28, 2018 at 07:00

    In case anyone else comes across this - fsdata_custom.c isn't meant to be directly compiled, it gets included in httpd/fs.c.  I removed fsdata_custom.c from my Makefile and the errors went away

    GreenGuy
    GreenGuyAuthor
    Senior III
    June 28, 2018
    Posted on June 28, 2018 at 19:07

    Ben, sorry for the late reply.  Yes you got it right.  For me I simply excluded the file from the build in the IDE.

    BROBL
    Visitor II
    October 25, 2018

    Hello Guys,

    I'm having the same problem when trying to build the example; my problem don't go away when I exclude that file from the build, I mean is replaced by a ..\Middlewares\Third_Party\LwIP\src\apps\httpd\fs.c:41:27: fatal error: fsdata_custom.c: No such file or directory

     #[include "fsdata_custom.c"]​ 

    Don't know if you would have any ideas

    Jona
    Associate III
    March 24, 2020

    I was able to get rid of the errors by including the fsdata.h file. But eventually just excluded fsdata_custom.c. I then ended up with 3 more fatal errors

    multiple definition of _isatty

    (2)Undefined reference to "missing_USE_FREERTOS_macro"

    It must be nearly IMPOSSIBLE for St to create examples that actually build and work as I have yet to see one.

    Adding "USE_FREERTOS" to the Project Properties solved one. But still have no solution for _isatty. Searching for it.. doesn't show up anywhere.