Skip to main content
GreenGuy
Senior III
Jul 6, 2018 11:39 PM UTC
Question

EXTI9_5_IRQHandler missing in CubeMX H743i_Eval Build

Posted on July 07, 2018 at 01:39

Trying to figure out reasons why a CubeMX build cannot replicate the functionality of the repo application:

STM32Cube\Repository\STM32Cube_FW_H7_V1.2.0\Projects\STM32H743I_EVAL\Applications\FatFs\FatFs_uSD_DMA_RTOS.

The CubeMX generation has the file operations code exactly matching the code found in the example project noted.  I found missing code in stm32h7xx_it.c built by CubeMX.  There is no handler for the SD Detect set up in stm32h743i_eval.c (see lines 1078 - 1100).  CubeMX contains all the board specific assignments and generates code to call the initializing function MFX_IO_ITConfig() so why leave out the interrupt handler.  I am sure this is an oversight.

It is fixed by adding to the end of stm32h7xx_it.c in the user section as shown:

/* USER CODE BEGIN 1 */

/**

  * @brief  This function handles SD detection interrupty

  * @param  None

  * @retval None

  */

void EXTI9_5_IRQHandler(void)

{

  SD_DetectIRQHandler();

}

/* USER CODE END 1 */

This is the same code used in the repo application example noted.

Now the application does not hang when the card is removed or inserted.

Unfortunately it does not fix the inability to open/read/write with out returning FR_NOT_READY!

    This topic has been closed for replies.

    3 replies

    ST Technical Moderator
    Jul 9, 2018 1:39 PM UTC
    Posted on July 09, 2018 at 15:39

    Hello

    greenwood.greg

    ,

    I raised this issue internally for check.

    Thank you for your contribution.

    With Regards,

    Imen

    In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
    Mohamed Mansouri
    Visitor II
    Jul 11, 2018 9:37 AM UTC
    Posted on July 11, 2018 at 11:37

    Hi

    greenwood.greg

     ,

    Thanks for your feedback,

    In fact, there are some differences in the project organization between those generated by cubeMX and those in the repository folder.

    As you can see, there are USER TAGs where user can add his own code depending on his requirements.

    With Regards,

    Mohamed

    GreenGuy
    GreenGuyAuthor
    Senior III
    Jul 11, 2018 6:27 PM UTC
    Posted on July 11, 2018 at 18:27

    What you say is true and is fixed in like manner, however, this code is not based on my own requirements but the requirements of the hardware and therefore should be added by CubeMX based on my selection of the eval board in CubeMX.