Associate III
January 16, 2016
Question
Input Capture module in pulse count example
- January 16, 2016
- 4 replies
- 1507 views
Posted on January 16, 2016 at 07:49
Hello all,
In an external pulse count application, is it possible to capture Timer counts at fixed interval using input capture (IC) module while external input (TIM5_CH1) is driving timer time-base (through TI1F_ED).
I've also tried just storing TIM5->CNT at every RTC interrupt, but found some irregular counts. May be this irregularity is for other interrupts (of high priority) with LP Sleep implementations.
I request some advice on how to configure this capture module (if possible on STML151, clock tree attached). I've configured TIM_5 like this:
......... ......... /* Reset the CC1E Bit to configure CC1S bit of CCMR1 Reg */ TIM5->CCER &= (uint16_t)~((uint16_t)TIM_CCER_CC1E); tmpccmr1 = TIM5->CCMR1; tmpccer = TIM5->CCER; /* TIM5 Input CH1 is selected to be connected to IC1. and reset the filter */ tmpccmr1 &= (uint16_t)(((uint16_t)~((uint16_t)TIM_CCMR1_CC1S)) & ((uint16_t)~((uint16_t)TIM_CCMR1_IC1F))); tmpccmr1 |= (uint16_t)(TIM_ICSelection_DirectTI | (uint16_t)(0x00 << (uint16_t)4)); /* IC Rising edge and set the CC1E Bit */ tmpccer &= (uint16_t)~((uint16_t)(TIM_CCER_CC1P | TIM_CCER_CC1NP));/* Write to TIM5 CCMR1 and CCER registers */
TIM5->CCMR1 = tmpccmr1; TIM5->CCER = tmpccer; //Input Trigger source TIM_TS_TI1F_ED: TI1 Edge Detector. TIM_SelectInputTrigger(TIM5, TIM_TS_TI1F_ED); //Slave Mode TIM_SlaveMode_External1: SMS=111 TIM_SelectSlaveMode(TIM5, TIM_SlaveMode_External1); /* TIM5 enable counter */ TIM_Cmd(TIM5, ENABLE);